Transport that uses RPMsg zero copy RTOS API for interprocessor messaging.
More...
#include <erpc_rpmsg_tty_rtos_transport.hpp>
Transport that uses RPMsg zero copy RTOS API for interprocessor messaging.
| RPMsgTTYRTOSTransport::RPMsgTTYRTOSTransport |
( |
void |
| ) |
|
Constructor.
This function initializes object attributes.
| erpc_status_t RPMsgTTYRTOSTransport::init |
( |
uint32_t |
src_addr, |
|
|
uint32_t |
dst_addr, |
|
|
void * |
base_address, |
|
|
uint32_t |
length, |
|
|
uint32_t |
rpmsg_link_id |
|
) |
| |
|
virtual |
This function call RPMsg rtos init function - as RPMsg master.
- Parameters
-
| [in] | src_addr | Source address. |
| [in] | dst_addr | Destination address. |
| [in] | base_address | RPMsg base address in the shared memory. |
| [in] | length | RPMsg shared memory region length. |
| [in] | rpmsg_link_id | Selection between what cores the communication will occur. |
- Return values
-
| kErpcStatus_Success | When rpmsg init function was executed successfully. |
| kErpcStatus_InitFailed | When rpmsg init function wasn't executed successfully. |
| erpc_status_t RPMsgTTYRTOSTransport::init |
( |
uint32_t |
src_addr, |
|
|
uint32_t |
dst_addr, |
|
|
void * |
base_address, |
|
|
uint32_t |
rpmsg_link_id, |
|
|
void(*)(void) |
ready_cb, |
|
|
char * |
nameservice_name |
|
) |
| |
|
virtual |
This function call RPMsg rtos init function - as RPMsg remote.
- Parameters
-
| [in] | src_addr | Source address. |
| [in] | dst_addr | Destination address. |
| [in] | base_address | RPMsg base address in the shared memory. |
| [in] | rpmsg_link_id | Selection between what cores the communication will occur. |
| [in] | ready_cb | Callback called after RPMsg init is done and the core is ready. |
| [in] | nameservice_name | Name of the nameservice channel to be announced to the other core. |
- Return values
-
| kErpcStatus_Success | When rpmsg init function was executed successfully. |
| kErpcStatus_InitFailed | When rpmsg init function wasn't executed successfully. |
Store incoming message to message buffer.
In loop while no message come.
- Parameters
-
| [in] | message | Message buffer, to which will be stored incoming message. |
- Return values
-
| kErpcStatus_ReceiveFailed | Failed to receive message buffer. |
| kErpcStatus_Success | Successfully received all data. |
Implements erpc::Transport.
Function to send prepared message.
- Parameters
-
| [in] | message | Pass message buffer to send. |
- Return values
-
| kErpcStatus_SendFailed | Failed to send message buffer. |
| kErpcStatus_Success | Successfully sent all data. |
Implements erpc::Transport.
| void RPMsgTTYRTOSTransport::setCrc16 |
( |
Crc16 * |
crcImpl | ) |
|
|
virtual |
This functions sets the CRC-16 implementation.
- Parameters
-
| [in] | crcImpl | Object containing crc-16 compute function. |
Reimplemented from erpc::Transport.
| Crc16 * RPMsgTTYRTOSTransport::getCrc16 |
( |
void |
| ) |
|
|
virtual |
This functions gets the CRC-16 object.
- Returns
- Crc16* Pointer to CRC-16 object containing crc-16 compute function.
Reimplemented from erpc::Transport.
| uint32_t erpc::RPMsgTTYRTOSTransport::m_dst_addr |
|
protected |
Destination address used by rpmsg.
| rpmsg_queue_handle erpc::RPMsgTTYRTOSTransport::m_rpmsg_queue |
|
protected |
| struct rpmsg_lite_endpoint* erpc::RPMsgTTYRTOSTransport::m_rpmsg_ept |
|
protected |
Pointer to RPMsg Lite Endpoint structure.
The documentation for this class was generated from the following files: