![]() |
eRPC Generator (erpcgen)
Rev. 1.11.0
NXP Semiconductors
|
Variable length list of another data type. More...
#include <ListType.hpp>
Public Member Functions | |
| ListType (DataType *elementType) | |
| Constructor. More... | |
| DataType * | getElementType () const |
| This function returns element data type. More... | |
| void | setElementType (DataType *elementType) |
| This function set element data type. More... | |
| virtual std::string | getDescription () const override |
| This function returns description about the list. More... | |
| void | setLengthVariableName (const std::string &lengthVariableName) |
| This function set variable name. This variable is used in generated file to store size of list. More... | |
| std::string & | getLengthVariableName () |
| This function returns variable name. This variable is used in generated file to store size of list. More... | |
| bool | hasLengthVariable () |
| This function returns information if object contains length variable. More... | |
Public Member Functions inherited from erpcgen::DataType | |
| DataType (data_type_t dataType) | |
| Constructor. More... | |
| DataType (const std::string &name, data_type_t dataType) | |
| Constructor. More... | |
| DataType (const Token &tok, data_type_t dataType) | |
| Constructor. More... | |
| data_type_t | getDataType () const |
| This function returns data type. More... | |
| DataType * | getTrueDataType () |
| This function returns pointer to true data type instead of alias. More... | |
| DataType * | getTrueContainerDataType () |
| This function returns pointer to true data type (enum, builtin, structs) except lists and arrays. More... | |
| bool | isAlias () const |
| This function is testing data type. More... | |
| bool | isArray () const |
| This function is testing data type. More... | |
| virtual bool | isBinary () const |
| This function return "false" value as default for identify binary type. More... | |
| virtual bool | isBool () const |
| This function return "false" value as default for identify bool type. More... | |
| bool | isBuiltin () const |
| This function is testing data type. More... | |
| bool | isEnum () const |
| This function is testing data type. More... | |
| bool | isFunction () const |
| This function is testing data type. More... | |
| bool | isList () const |
| This function is testing data type. More... | |
| virtual bool | isScalar () const |
| This function return "false" value as default for identify scalar builtin type. More... | |
| virtual bool | isInt () const |
| This function return "true" value for identify int type. More... | |
| virtual bool | isFloat () const |
| This function return "true" value for identify float type. More... | |
| virtual bool | isString () const |
| This function return "false" value as default for identify string type. More... | |
| virtual bool | isUString () const |
| This function return "false" value as default for identify ustring type. More... | |
| bool | isStruct () const |
| This function is testing data type. More... | |
| bool | isUnion () const |
| This function is testing data type. More... | |
| bool | isVoid () const |
| This function is testing data type. More... | |
Public Member Functions inherited from erpcgen::Symbol | |
| Symbol (symbol_type_t symType) | |
| Constructor. More... | |
| Symbol (symbol_type_t symType, const std::string &name) | |
| Constructor. More... | |
| Symbol (symbol_type_t symType, const Token &tok) | |
| Constructor. More... | |
| virtual | ~Symbol () |
| Destructor. | |
| symbol_type_t | getSymbolType () const |
| This function returns symbol type. More... | |
| const std::string & | getName () const |
| This function returns symbol name. More... | |
| void | setName (const std::string &newName) |
| This function set symbol name. More... | |
| bool | isConstSymbol () const |
| This function is testing symbol type. More... | |
| bool | isEnumMemberSymbol () const |
| This function is testing symbol type. More... | |
| bool | isFunctionSymbol () const |
| This function is testing symbol type. More... | |
| bool | isInterfaceSymbol () const |
| This function is testing symbol type. More... | |
| bool | isProgramSymbol () const |
| This function is testing symbol type. More... | |
| bool | isStructMemberSymbol () const |
| This function is testing symbol type. More... | |
| bool | isDatatypeSymbol () const |
| This function is testing symbol type. More... | |
| bool | isUnionCaseSymbol () const |
| This function is testing symbol type. More... | |
| token_loc_t & | getLocation () |
| This function returns location for symbol. More... | |
| void | setLocation (const token_loc_t &loc) |
| This function set location for symbol. More... | |
| int | getFirstLine () const |
| This function return first line from location of symbol. More... | |
| int | getLastLine () const |
| This function return last line from location of symbol. More... | |
| void | addAnnotation (const Annotation &a) |
| This function add annotation to vector of symbol annotations. More... | |
| std::string | printAnnotations () |
| This function returns description about annotation. More... | |
| Annotation * | findAnnotation (const std::string &name, Annotation::program_lang_t lang) |
| Find annotation in the annotation list. More... | |
| std::vector< Annotation * > | getAnnotations (const std::string &name, Annotation::program_lang_t lang) |
| Find annotations matching name in the annotation list. More... | |
| const std::vector< Annotation > & | getAnnotations () const |
| Return all Symbol annotations. More... | |
| Value * | getAnnValue (const std::string &annName, Annotation::program_lang_t lang) |
| This function search and returns Value object for given annotation name. More... | |
| std::string | getAnnStringValue (const std::string &annName, Annotation::program_lang_t lang) |
| This function search and returns string for given annotation name. More... | |
| std::string | getMlComment () |
| This function returns multiline comment for this symbol declared in IDL file. More... | |
| void | setMlComment (const std::string &comment) |
| This function set multiline comment for this symbol declared in IDL file. More... | |
| std::string | getIlComment () |
| This function returns inline comment for this symbol declared in IDL file. More... | |
| void | setIlComment (const std::string &comment) |
| This function set inline comment for this symbol declared in IDL file. More... | |
Protected Attributes | |
| DataType * | m_elementType |
| std::string | m_lengthVariableName |
Protected Attributes inherited from erpcgen::DataType | |
| data_type_t | m_dataType |
Protected Attributes inherited from erpcgen::Symbol | |
| symbol_type_t | m_symbolType |
| std::string | m_name |
| token_loc_t | m_location |
| std::vector< Annotation > | m_annotations |
| std::string | m_mlComment |
| std::string | m_ilComment |
Additional Inherited Members | |
Public Types inherited from erpcgen::DataType | |
| enum | data_type_t { kAliasType, kArrayType, kBuiltinType, kEnumType, kFunctionType, kListType, kStructType, kUnionType, kVoidType } |
| Supported data types. | |
Public Types inherited from erpcgen::Symbol | |
| enum | symbol_type_t { kConstSymbol, kEnumMemberSymbol, kFunctionSymbol, kInterfaceSymbol, kProgramSymbol, kStructMemberSymbol, kTypenameSymbol, kUnionCaseMemberSymbol } |
| Supported symbol types. | |
Variable length list of another data type.
|
inlineexplicit |
Constructor.
This function set element type to given data type.
| [in] | elementType | Given data type. |
|
overridevirtual |
This function returns description about the list.
Reimplemented from erpcgen::Symbol.
|
inline |
This function returns element data type.
|
inline |
This function returns variable name. This variable is used in generated file to store size of list.
|
inline |
This function returns information if object contains length variable.
| true | When list contains length variable. |
| false | When list doesn't contain length variable. |
|
inline |
This function set element data type.
| [in] | elementType | Element data type. |
|
inline |
This function set variable name. This variable is used in generated file to store size of list.
| [in] | lengthVariableName | Given name for variable. |
|
protected |
List element data type.
|
protected |
List length variable name.