Overview
========
The mco_manager/mcofd_manager example implements a minimal CANopen Manager.
It produces a cyclic heartbeat message (701h) and waits for 
CANopen Slave devices with a node ID in the range of 2 to 10.
Once a CiA 401 compatible generic I/O device is found,
the manager echos data received by the 401 device.

NOTE: For more details, please see the User's Manual for the
EmSA CANopen (FD) Libraries for NXP SDKs.


Implementation Description
Node-ID: 0x01, Baudrate: 500kbps

Messages produced (by CAN ID):
0x000       - NMT Master command message
0x602-0x60A - SDO requests to nodes 2 to 10
0x701       - Heartbeat (default 333ms)
Once a CiA 401 device is found with node ID nid:
0x200+nid   - RPDO1 of nid - Total of 4 input Bytes
    [6000h,1] Digital in byte 1: 0
    [6000h,2] Digital in byte 2: 0
    [6000h,3] Digital in byte 3: copy/echo of [6200h,1] Digital out byte 1
    [6000h,4] Digital in byte 4: copy/echo of [6200h,2] Digital out byte 2
0x300+nid   - RPDO2 of nid - Two 16-bit analog inputs
    [6401h,1] Analog out word16 1: timer with hi byte seconds and lo byte quarter seconds
    [6401h,2] Analog out word16 2: copy/echo of [6411h,2] Analog out word16 1

Messages consumed (by CAN ID):
0x082-0x0AA - Emergencies of nodes 2 to 10
0x582-0x58A - SDO responses to nodes 2 to 10
0x702-0x70A - Bootup and heartbeats of nodes 2 to 10
Once a CiA 401 device is found with node ID nid:
0x180+nid   - TPDO1 of nid - Four bytes of digital outputs. 
0x280+nid   - TPDO2 of nid - Two 16-bit analog outputs.

User can use a CAN monitor (USB CAN analysis) to probe the CAN frame transfered.
- CANL in CAN USB analysis connected with CANL in two board by shunt-wound method.
- CANH in CAN USB analysis connected with CANH in two board by shunt-wound method.
- (optinal) GND in CAN USB analysis connected with GND in two board by shunt-wound method.

Toolchain supported
===================
- IAR embedded Workbench  9.20.1
- Keil MDK  5.34
- GCC ARM Embedded  10.2.1
- MCUXpresso  11.4.1

Hardware requirements
=====================
- Two Micro USB cables
- Two LPCXpresso55S36 boards
- Personal Computer

Board settings
==============
Between CAN transceivers:
- CANH, CANL, GND should be connected
The jumper setting:
    Default jumpers configuration does not work,  you will need to add JP48 1-2, JP23 and JP24


Prepare the Demo
================
1.  Connect a micro USB cable between the host PC and the LPC-Link USB port (J1) on the target board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo
================
1. First press the reset button on the board with the mcofd_slave example
2. Second press the reset button on the board with the mcofd_manager example

~~~~~~~~~~~~~~~~~~~~~
The terminal connected to the mcofd_manager example displays similar like that:

Starting CANopen FD Library manager example
Provided by EmSA - www.em-sa.com/nxp

CANopen FD Library Event - Reset Communication, nominal bitrate 500kbps, data bitrate 2000kbps, node id 1
CANopen FD Library Event - NMT Change: 0x 0 boot 
CANopen FD Library Event - NMT Change: 0x 5 operational 
CANopen FD Manager Event - Node Status Change: 3, 0x 0 booted 
CANopen FD Manager Event - Node Status Change: 3, 0x81 emergency over / reset 
CANopen FD Manager Event - Node Status Change: 3, 0xA0 scan complete
 [1000,01]:   F0191 [1018,01]:AF0002DC [1018,02]:C0DE0020 
CANopen FD Manager Event - Node Status Change: 3, 0x 5 operational 
CANopen FD Manager Event - Node Status Change: 3, 0x90 heartbeat monitoring active 
CANopen FD Manager USDO Client Complete: node 3
 [1008,00]:CANopenLibNXPSDK CiA401-B/F Example
 

The terminal connected to the mcofd_slave example displays similar like that:

Starting CANopen FD Library slave example
Provided by EmSA - www.em-sa.com/nxp

CANopen FD Library Event - Reset Communication, nominal bitrate 500kbps, data bitrate 2000kbps, node id 3 
CANopen FD Library Event - NMT Change: 0x 0 boot 
CANopen FD Library Event - NMT Change: 0x7F pre-operational 
CANopen FD Library Event - NMT Change: 0x7F pre-operational 
CANopen FD Library Event - NMT Change: 0x 5 operational 
~~~~~~~~~~~~~~~~~~~~~