Overview
========
The SCTimer 16-bit counter project is a demonstration program of the SDK SCTimer driver operation when using the SCTimer counter
as two 16-bit counters.
The example toggles an output per counter when a match occurs.

Toolchain supported
===================
- IAR embedded Workbench  9.20.1
- Keil MDK  5.34
- GCC ARM Embedded  10.2.1
- MCUXpresso  11.4.1

Hardware requirements
=====================
- Micro USB cable
- LPCXpresso55S36 board
- Personal Computer

# Board settings

```
Output signal		Board location
SCT0_OUT0    		J10-5 (P1_4)
SCT0_OUT4    		J10-13(P1_17)
```

# Prepare the Demo

1.  Connect a micro USB cable between the host PC and the LPC-Link USB port (J1) on the target board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo
================
The log below shows example output in the terminal window:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
SCTimer example to use it in 16-bit mode
The example shows both 16-bit counters running and toggling an output periodically
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

You'll see PWM signals on J10-5 and J10-13 using an oscilloscope