Overview
========
The iperf3 example provides basic commands to measure performance of network stack.
Results will be shown on your iperf server. In the case of 'R' mode, server shows the amount of sent data,
check the terminal output in this case for the total amount of payload in bytes received over UDP,
which marks the device's throughput.

Known Issues
If the iperf3 server shows you that you have 0-bit/s bandwidth, it may be caused due to the version you are using.
This client works with Iperf v3.7. In case of any more issues, see https://github.com/esnet/iperf/labels/bug. 

Rx UDP mode ('R') has limited bandwidth by UDP_RX_BANDWIDTH macro as sending UDP packets too fast may cause
the control TCP socket to lost data and test failure.
Set the macro to a little bit higher than the device can receive or "0" for no limit.

The network throughput is limited by UART interface between board and Wi-Fi module. Default UART speed is set to 115200 Bd.


Toolchain supported
===================
- IAR embedded Workbench  9.20.1
- Keil MDK  5.34
- GCC ARM Embedded  10.2.1
- MCUXpresso  11.4.1

Hardware requirements
=====================
- Mini/micro USB cable
- LPCXpresso55S36 board
- Personal Computer
- Murata CMWC1ZZABR-107-EVB

Board settings
==============
Make sure the JP52 is in position 1-2.

Plug the Wi-Fi module to mikroBUS (J7, J8).

Prepare the Demo
================
1.  Prepare iperf3 server on your machine:
    - Install iperf3 (Enter command "sudo apt install iperf3")
    - Start the server by running "iperf3 -s"
2.  Connect a micro USB cable between the PC host and the SDA port
3.  Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Reset the SoC and run the project.
5.  During the runtime will be necessary to configure Wi-Fi module. Follow instructions in the terminal for Wi-Fi module configuration or resetting to provisioning mode.
    If the module is in provisioning mode, it will create micro-AP:
        SSID: Serial2Wifi
        Passphrase: nxp12345
    Connect your PC or mobile phone to this Wi-Fi micro-AP, open address: http://192.168.10.1 in web browser, select "Provisioning" and then select WLAN for connection.
    Wi-Fi module stores the WLAN credentials and it will use them automatically for next connection.

Running the demo
================
When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Enter IP address of a server in format '192.168.1.2'
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Enter IP address of the iperf3 server.

~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Using IP xxx.xxx.xxx.xxx
Menu:
Press 's' to start client Tx mode
Press 'r' to start client Rx mode
Press 'S' to start client Tx UDP mode
Press 'R' to start client Rx UDP mode
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~

- Press 's' to start Iperf3 client in sending mode. (TCP)
- Press 'r' to start Iperf3 client in receiving mode. (TCP)
- Press 'S' to start Iperf3 client in sending mode. (UDP)
- Press 'R' to start Iperf3 client in receiving mode. (UDP)