Example AES-128 ECB encryption using the CSSv2 (CLNS component mcuxClCss) More...
Functions | |
| bool | cipher_aes128_ecb_encrypt (void) |
| Performs AES-128 ECB encryption using mcuxClCss functions. More... | |
Variables | |
| static uint8_t const | aes128_input [MCUXCLCSS_CIPHER_BLOCK_SIZE_AES] |
| Plaintext input for the AES encryption. More... | |
| static uint8_t const | aes128_expected_output [MCUXCLCSS_CIPHER_BLOCK_SIZE_AES] |
| Expected ciphertext output of the AES encryption. More... | |
| static uint8_t const | aes128_key [MCUXCLCSS_CIPHER_KEY_SIZE_AES_128] |
| Key for the AES encryption. More... | |
| static uint8_t | aes128_output [MCUXCLCSS_CIPHER_BLOCK_SIZE_AES] |
| Destination buffer to receive the ciphertext output of the AES encryption. More... | |
Example AES-128 ECB encryption using the CSSv2 (CLNS component mcuxClCss)
| bool cipher_aes128_ecb_encrypt | ( | void | ) |
Performs AES-128 ECB encryption using mcuxClCss functions.
| true | The example code completed successfully |
| false | The example code failed |
|
static |
Plaintext input for the AES encryption.
|
static |
Expected ciphertext output of the AES encryption.
|
static |
Key for the AES encryption.
|
static |
Destination buffer to receive the ciphertext output of the AES encryption.