Option values for mcuxClCss_CmacOption_t. More...
Macros | |
| #define | MCUXCLCSS_CMAC_EXTERNAL_KEY_ENABLE |
| Set mcuxClCss_CmacOption_t.extkey to this value to use an external key. More... | |
| #define | MCUXCLCSS_CMAC_EXTERNAL_KEY_DISABLE |
| Set mcuxClCss_CmacOption_t.extkey to this value to use a key from the CSSv2 keystore. More... | |
| #define | MCUXCLCSS_CMAC_INITIALIZE_DISABLE |
| Set mcuxClCss_CmacOption_t.initialize to this value if the message chunk does not include the first block of the message. More... | |
| #define | MCUXCLCSS_CMAC_INITIALIZE_ENABLE |
| Set mcuxClCss_CmacOption_t.initialize to this value if the message chunk includes the first block of the message. More... | |
| #define | MCUXCLCSS_CMAC_FINALIZE_DISABLE |
| Set mcuxClCss_CmacOption_t.finalize to this value if the message chunk does not include the last block of the message. More... | |
| #define | MCUXCLCSS_CMAC_FINALIZE_ENABLE |
| Set mcuxClCss_CmacOption_t.finalize to this value if the message chunk includes the last block of the message. More... | |
| #define | MCUXCLCSS_CMAC_STATE_IN_DISABLE |
| Set mcuxClCss_CmacOption_t.sie to this value to use the CMAC state that is present inside CSS. More... | |
| #define | MCUXCLCSS_CMAC_STATE_IN_ENABLE |
| Set mcuxClCss_CmacOption_t.sie to this value to import the CMAC state from memory. More... | |
| #define | MCUXCLCSS_CMAC_STATE_OUT_DISABLE |
| Set mcuxClCss_CmacOption_t.soe to this value to keep the CMAC state inside CSS at the end of the command. More... | |
| #define | MCUXCLCSS_CMAC_STATE_OUT_ENABLE |
| Set mcuxClCss_CmacOption_t.soe to this value to export the CMAC state to memory at the end of the command. More... | |
Option values for mcuxClCss_CmacOption_t.
| #define MCUXCLCSS_CMAC_EXTERNAL_KEY_ENABLE |
Set mcuxClCss_CmacOption_t.extkey to this value to use an external key.
| #define MCUXCLCSS_CMAC_EXTERNAL_KEY_DISABLE |
Set mcuxClCss_CmacOption_t.extkey to this value to use a key from the CSSv2 keystore.
| #define MCUXCLCSS_CMAC_INITIALIZE_DISABLE |
Set mcuxClCss_CmacOption_t.initialize to this value if the message chunk does not include the first block of the message.
| #define MCUXCLCSS_CMAC_INITIALIZE_ENABLE |
Set mcuxClCss_CmacOption_t.initialize to this value if the message chunk includes the first block of the message.
| #define MCUXCLCSS_CMAC_FINALIZE_DISABLE |
Set mcuxClCss_CmacOption_t.finalize to this value if the message chunk does not include the last block of the message.
| #define MCUXCLCSS_CMAC_FINALIZE_ENABLE |
Set mcuxClCss_CmacOption_t.finalize to this value if the message chunk includes the last block of the message.
| #define MCUXCLCSS_CMAC_STATE_IN_DISABLE |
Set mcuxClCss_CmacOption_t.sie to this value to use the CMAC state that is present inside CSS.
| #define MCUXCLCSS_CMAC_STATE_IN_ENABLE |
Set mcuxClCss_CmacOption_t.sie to this value to import the CMAC state from memory.
| #define MCUXCLCSS_CMAC_STATE_OUT_DISABLE |
Set mcuxClCss_CmacOption_t.soe to this value to keep the CMAC state inside CSS at the end of the command.
| #define MCUXCLCSS_CMAC_STATE_OUT_ENABLE |
Set mcuxClCss_CmacOption_t.soe to this value to export the CMAC state to memory at the end of the command.