Constants for initalizing mcuxClCss_KeyProp_t.bits. More...
Macros | |
| #define | MCUXCLCSS_KEYPROPERTY_KEY_SIZE_128 |
| This value of mcuxClCss_KeyProp_t.ksize indicates a 128 bit key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_KEY_SIZE_256 |
| This value of mcuxClCss_KeyProp_t.ksize indicates a 256 bit key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_ACTIVE_TRUE |
| This value of mcuxClCss_KeyProp_t.kactv indicates that the slot contains an active key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_ACTIVE_FALSE |
| This value of mcuxClCss_KeyProp_t.kactv indicates that the slot does not contain active key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_BASE_SLOT |
| This value of mcuxClCss_KeyProp_t.kbase indicates that the slot is the base slot of a 2-slot key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_SECOND_SLOT |
| This value of mcuxClCss_KeyProp_t.kbase indicates that the slot is the second slot of a 2-slot key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_GENERAL_PURPOSE_SLOT_TRUE |
| This value of mcuxClCss_KeyProp_t.fgp indicates that the slot is a retention key slot or a hardware out key slot. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_GENERAL_PURPOSE_SLOT_FALSE |
| This value of mcuxClCss_KeyProp_t.fgp indicates that the slot is a neither retention key slot nor hardware out key slot. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_RETENTION_SLOT_TRUE |
| This value of mcuxClCss_KeyProp_t.frtn indicates that the slot is a retention key slot. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_RETENTION_SLOT_FALSE |
| This value of mcuxClCss_KeyProp_t.frtn indicates that the slot is not a retention key slot. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_HW_OUT_SLOT_TRUE |
| This value of mcuxClCss_KeyProp_t.fhwo indicates that the slot is a hardware out key slot. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_HW_OUT_SLOT_FALSE |
| This value of mcuxClCss_KeyProp_t.fhwo indicates that the slot is not a hardware out key slot. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_CMAC_TRUE |
| This value of mcuxClCss_KeyProp_t.ucmac indicates that the key can be used for CMAC. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_CMAC_FALSE |
| This value of mcuxClCss_KeyProp_t.ucmac indicates that the key cannot be used for CMAC. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_KSK_TRUE |
| This value of mcuxClCss_KeyProp_t.uksk indicates that the key can be used for key signing. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_KSK_FALSE |
| This value of mcuxClCss_KeyProp_t.uksk indicates that the key cannot be used for key signing. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_RTF_TRUE |
| This value of mcuxClCss_KeyProp_t.urtf indicates that the key can be used for RTF signing. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_RTF_FALSE |
| This value of mcuxClCss_KeyProp_t.urtf indicates that the key cannot be used for RTF signing. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_CKDF_TRUE |
| This value of mcuxClCss_KeyProp_t.uckdf indicates that the key can be used for CKDF. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_CKDF_FALSE |
| This value of mcuxClCss_KeyProp_t.uckdf indicates that the key cannot be used for CKDF. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_HKDF_TRUE |
| This value of mcuxClCss_KeyProp_t.uhkdf indicates that the key can be used for HKDF. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_HKDF_FALSE |
| This value of mcuxClCss_KeyProp_t.uhkdf indicates that the key cannot be used for HKDF. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_ECC_TRUE |
| This value of mcuxClCss_KeyProp_t.uecsg indicates that the key can be used for ECC signing. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_ECC_FALSE |
| This value of mcuxClCss_KeyProp_t.uecsg indicates that the key cannot be used for ECC signing. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_ECC_DH_PRIVATE_TRUE |
| This value of mcuxClCss_KeyProp_t.uecdh indicates that the key is a ECC Diffie Hellman private key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_ECC_DH_PRIVATE_FALSE |
| This value of mcuxClCss_KeyProp_t.uecdh indicates that the key is not an ECC Diffie Hellman private key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_AES_TRUE |
| This value of mcuxClCss_KeyProp_t.uaes indicates that the key is an AES key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_AES_FALSE |
| This value of mcuxClCss_KeyProp_t.uaes indicates that the key is not an AES key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_HMAC_TRUE |
| This value of mcuxClCss_KeyProp_t.uhmac indicates that the key is an HMAC key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_HMAC_FALSE |
| This value of mcuxClCss_KeyProp_t.uhmac indicates that the key is not an HMAC key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_KWK_TRUE |
| This value of mcuxClCss_KeyProp_t.ukwk indicates that the key is a Key Wrapping Key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_KWK_FALSE |
| This value of mcuxClCss_KeyProp_t.ukwk indicates that the key is not a Key Wrapping Key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_KUOK_TRUE |
| This value of mcuxClCss_KeyProp_t.ukuok indicates that the key is a Key Unwrapping Only Key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_KUOK_FALSE |
| This value of mcuxClCss_KeyProp_t.ukuok indicates that the key is not a Key Unwrapping Only Key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_TLS_PREMASTER_SECRET_TRUE |
| This value of mcuxClCss_KeyProp_t.utlspms indicates that the key is a TLS Premaster Secret. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_TLS_PREMASTER_SECRET_FALSE |
| This value of mcuxClCss_KeyProp_t.utlspms indicates that the key is not a TLS Premaster Secret. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_TLS_MASTER_SECRET_TRUE |
| This value of mcuxClCss_KeyProp_t.utlsms indicates that the key is a TLS Master Secret. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_TLS_MASTER_SECRET_FALSE |
| This value of mcuxClCss_KeyProp_t.utlsms indicates that the key is not a TLS Master Secret. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_INPUT_FOR_ECC_TRUE |
| This value of mcuxClCss_KeyProp_t.ukgsrc indicates that the key can be used as key material input for ECC key generation. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_INPUT_FOR_ECC_FALSE |
| This value of mcuxClCss_KeyProp_t.ukgsrc indicates that the key cannot be used as key material input for ECC key generation. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_HW_OUT_TRUE |
| This value of mcuxClCss_KeyProp_t.uhwo indicates that the key can be used in a hardware out key slot. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_HW_OUT_FALSE |
| This value of mcuxClCss_KeyProp_t.uhwo indicates that the key cannot be used in a hardware out key slot. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_WRAP_TRUE |
| This value of mcuxClCss_KeyProp_t.wrpok indicates that the key can be wrapped. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_WRAP_FALSE |
| This value of mcuxClCss_KeyProp_t.wrpok indicates that the key cannot be wrapped. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_DEVICE_UNIQUE_TRUE |
| This value of mcuxClCss_KeyProp_t.duk indicates that the key is a Device Unique Key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_DEVICE_UNIQUE_FALSE |
| This value of mcuxClCss_KeyProp_t.duk indicates that the key is not a Device Unique Key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_PRIVILEGED_TRUE |
| This value of mcuxClCss_KeyProp_t.upprot_priv indicates that the caller must be in privileged mode to use the key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_PRIVILEGED_FALSE |
| This value of mcuxClCss_KeyProp_t.upprot_priv indicates that the caller does not need to be in privileged mode to use the key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_SECURE_TRUE |
| This value of mcuxClCss_KeyProp_t.upprot_sec indicates that the caller must be in secure mode to use the key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_SECURE_FALSE |
| This value of mcuxClCss_KeyProp_t.upprot_sec indicates that the caller does not need to be in secure mode to use the key. More... | |
Constants for initalizing mcuxClCss_KeyProp_t.bits.
| #define MCUXCLCSS_KEYPROPERTY_KEY_SIZE_128 |
This value of mcuxClCss_KeyProp_t.ksize indicates a 128 bit key.
| #define MCUXCLCSS_KEYPROPERTY_KEY_SIZE_256 |
This value of mcuxClCss_KeyProp_t.ksize indicates a 256 bit key.
| #define MCUXCLCSS_KEYPROPERTY_ACTIVE_TRUE |
This value of mcuxClCss_KeyProp_t.kactv indicates that the slot contains an active key.
| #define MCUXCLCSS_KEYPROPERTY_ACTIVE_FALSE |
This value of mcuxClCss_KeyProp_t.kactv indicates that the slot does not contain active key.
| #define MCUXCLCSS_KEYPROPERTY_BASE_SLOT |
This value of mcuxClCss_KeyProp_t.kbase indicates that the slot is the base slot of a 2-slot key.
| #define MCUXCLCSS_KEYPROPERTY_SECOND_SLOT |
This value of mcuxClCss_KeyProp_t.kbase indicates that the slot is the second slot of a 2-slot key.
| #define MCUXCLCSS_KEYPROPERTY_GENERAL_PURPOSE_SLOT_TRUE |
This value of mcuxClCss_KeyProp_t.fgp indicates that the slot is a retention key slot or a hardware out key slot.
| #define MCUXCLCSS_KEYPROPERTY_GENERAL_PURPOSE_SLOT_FALSE |
This value of mcuxClCss_KeyProp_t.fgp indicates that the slot is a neither retention key slot nor hardware out key slot.
| #define MCUXCLCSS_KEYPROPERTY_RETENTION_SLOT_TRUE |
This value of mcuxClCss_KeyProp_t.frtn indicates that the slot is a retention key slot.
| #define MCUXCLCSS_KEYPROPERTY_RETENTION_SLOT_FALSE |
This value of mcuxClCss_KeyProp_t.frtn indicates that the slot is not a retention key slot.
| #define MCUXCLCSS_KEYPROPERTY_HW_OUT_SLOT_TRUE |
This value of mcuxClCss_KeyProp_t.fhwo indicates that the slot is a hardware out key slot.
| #define MCUXCLCSS_KEYPROPERTY_HW_OUT_SLOT_FALSE |
This value of mcuxClCss_KeyProp_t.fhwo indicates that the slot is not a hardware out key slot.
| #define MCUXCLCSS_KEYPROPERTY_CMAC_TRUE |
This value of mcuxClCss_KeyProp_t.ucmac indicates that the key can be used for CMAC.
| #define MCUXCLCSS_KEYPROPERTY_CMAC_FALSE |
This value of mcuxClCss_KeyProp_t.ucmac indicates that the key cannot be used for CMAC.
| #define MCUXCLCSS_KEYPROPERTY_KSK_TRUE |
This value of mcuxClCss_KeyProp_t.uksk indicates that the key can be used for key signing.
| #define MCUXCLCSS_KEYPROPERTY_KSK_FALSE |
This value of mcuxClCss_KeyProp_t.uksk indicates that the key cannot be used for key signing.
| #define MCUXCLCSS_KEYPROPERTY_RTF_TRUE |
This value of mcuxClCss_KeyProp_t.urtf indicates that the key can be used for RTF signing.
| #define MCUXCLCSS_KEYPROPERTY_RTF_FALSE |
This value of mcuxClCss_KeyProp_t.urtf indicates that the key cannot be used for RTF signing.
| #define MCUXCLCSS_KEYPROPERTY_CKDF_TRUE |
This value of mcuxClCss_KeyProp_t.uckdf indicates that the key can be used for CKDF.
| #define MCUXCLCSS_KEYPROPERTY_CKDF_FALSE |
This value of mcuxClCss_KeyProp_t.uckdf indicates that the key cannot be used for CKDF.
| #define MCUXCLCSS_KEYPROPERTY_HKDF_TRUE |
This value of mcuxClCss_KeyProp_t.uhkdf indicates that the key can be used for HKDF.
| #define MCUXCLCSS_KEYPROPERTY_HKDF_FALSE |
This value of mcuxClCss_KeyProp_t.uhkdf indicates that the key cannot be used for HKDF.
| #define MCUXCLCSS_KEYPROPERTY_ECC_TRUE |
This value of mcuxClCss_KeyProp_t.uecsg indicates that the key can be used for ECC signing.
| #define MCUXCLCSS_KEYPROPERTY_ECC_FALSE |
This value of mcuxClCss_KeyProp_t.uecsg indicates that the key cannot be used for ECC signing.
| #define MCUXCLCSS_KEYPROPERTY_ECC_DH_PRIVATE_TRUE |
This value of mcuxClCss_KeyProp_t.uecdh indicates that the key is a ECC Diffie Hellman private key.
| #define MCUXCLCSS_KEYPROPERTY_ECC_DH_PRIVATE_FALSE |
This value of mcuxClCss_KeyProp_t.uecdh indicates that the key is not an ECC Diffie Hellman private key.
| #define MCUXCLCSS_KEYPROPERTY_AES_TRUE |
This value of mcuxClCss_KeyProp_t.uaes indicates that the key is an AES key.
| #define MCUXCLCSS_KEYPROPERTY_AES_FALSE |
This value of mcuxClCss_KeyProp_t.uaes indicates that the key is not an AES key.
| #define MCUXCLCSS_KEYPROPERTY_HMAC_TRUE |
This value of mcuxClCss_KeyProp_t.uhmac indicates that the key is an HMAC key.
| #define MCUXCLCSS_KEYPROPERTY_HMAC_FALSE |
This value of mcuxClCss_KeyProp_t.uhmac indicates that the key is not an HMAC key.
| #define MCUXCLCSS_KEYPROPERTY_KWK_TRUE |
This value of mcuxClCss_KeyProp_t.ukwk indicates that the key is a Key Wrapping Key.
| #define MCUXCLCSS_KEYPROPERTY_KWK_FALSE |
This value of mcuxClCss_KeyProp_t.ukwk indicates that the key is not a Key Wrapping Key.
| #define MCUXCLCSS_KEYPROPERTY_KUOK_TRUE |
This value of mcuxClCss_KeyProp_t.ukuok indicates that the key is a Key Unwrapping Only Key.
| #define MCUXCLCSS_KEYPROPERTY_KUOK_FALSE |
This value of mcuxClCss_KeyProp_t.ukuok indicates that the key is not a Key Unwrapping Only Key.
| #define MCUXCLCSS_KEYPROPERTY_TLS_PREMASTER_SECRET_TRUE |
This value of mcuxClCss_KeyProp_t.utlspms indicates that the key is a TLS Premaster Secret.
| #define MCUXCLCSS_KEYPROPERTY_TLS_PREMASTER_SECRET_FALSE |
This value of mcuxClCss_KeyProp_t.utlspms indicates that the key is not a TLS Premaster Secret.
| #define MCUXCLCSS_KEYPROPERTY_TLS_MASTER_SECRET_TRUE |
This value of mcuxClCss_KeyProp_t.utlsms indicates that the key is a TLS Master Secret.
| #define MCUXCLCSS_KEYPROPERTY_TLS_MASTER_SECRET_FALSE |
This value of mcuxClCss_KeyProp_t.utlsms indicates that the key is not a TLS Master Secret.
| #define MCUXCLCSS_KEYPROPERTY_INPUT_FOR_ECC_TRUE |
This value of mcuxClCss_KeyProp_t.ukgsrc indicates that the key can be used as key material input for ECC key generation.
| #define MCUXCLCSS_KEYPROPERTY_INPUT_FOR_ECC_FALSE |
This value of mcuxClCss_KeyProp_t.ukgsrc indicates that the key cannot be used as key material input for ECC key generation.
| #define MCUXCLCSS_KEYPROPERTY_HW_OUT_TRUE |
This value of mcuxClCss_KeyProp_t.uhwo indicates that the key can be used in a hardware out key slot.
| #define MCUXCLCSS_KEYPROPERTY_HW_OUT_FALSE |
This value of mcuxClCss_KeyProp_t.uhwo indicates that the key cannot be used in a hardware out key slot.
| #define MCUXCLCSS_KEYPROPERTY_WRAP_TRUE |
This value of mcuxClCss_KeyProp_t.wrpok indicates that the key can be wrapped.
| #define MCUXCLCSS_KEYPROPERTY_WRAP_FALSE |
This value of mcuxClCss_KeyProp_t.wrpok indicates that the key cannot be wrapped.
| #define MCUXCLCSS_KEYPROPERTY_DEVICE_UNIQUE_TRUE |
This value of mcuxClCss_KeyProp_t.duk indicates that the key is a Device Unique Key.
| #define MCUXCLCSS_KEYPROPERTY_DEVICE_UNIQUE_FALSE |
This value of mcuxClCss_KeyProp_t.duk indicates that the key is not a Device Unique Key.
| #define MCUXCLCSS_KEYPROPERTY_PRIVILEGED_TRUE |
This value of mcuxClCss_KeyProp_t.upprot_priv indicates that the caller must be in privileged mode to use the key.
| #define MCUXCLCSS_KEYPROPERTY_PRIVILEGED_FALSE |
This value of mcuxClCss_KeyProp_t.upprot_priv indicates that the caller does not need to be in privileged mode to use the key.
| #define MCUXCLCSS_KEYPROPERTY_SECURE_TRUE |
This value of mcuxClCss_KeyProp_t.upprot_sec indicates that the caller must be in secure mode to use the key.
| #define MCUXCLCSS_KEYPROPERTY_SECURE_FALSE |
This value of mcuxClCss_KeyProp_t.upprot_sec indicates that the caller does not need to be in secure mode to use the key.