Defines all functions of mcuxClCss_Aead. More...
Functions | |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t | mcuxClCss_Aead_Init_Async (mcuxClCss_AeadOption_t options, mcuxClCss_KeyIndex_t keyIdx, uint8_t const *pKey, size_t keyLength, uint8_t const *pIV, size_t ivLength, uint8_t *pAeadCtx) |
| AES-GCM initialization. More... | |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t | mcuxClCss_Aead_PartialInit_Async (mcuxClCss_AeadOption_t options, mcuxClCss_KeyIndex_t keyIdx, uint8_t const *pKey, size_t keyLength, uint8_t const *pIV, size_t ivLength, uint8_t *pAeadCtx) |
| AES-GCM partial initialization. More... | |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t | mcuxClCss_Aead_UpdateAad_Async (mcuxClCss_AeadOption_t options, mcuxClCss_KeyIndex_t keyIdx, uint8_t const *pKey, size_t keyLength, uint8_t const *pAad, size_t aadLength, uint8_t *pAeadCtx) |
| AES-GCM update of the Additional Authenticated Data (AAD) More... | |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t | mcuxClCss_Aead_UpdateData_Async (mcuxClCss_AeadOption_t options, mcuxClCss_KeyIndex_t keyIdx, uint8_t const *pKey, size_t keyLength, uint8_t const *pInput, size_t inputLength, uint8_t *pOutput, uint8_t *pAeadCtx) |
| AES-GCM update of the encrypted data. More... | |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t | mcuxClCss_Aead_Finalize_Async (mcuxClCss_AeadOption_t options, mcuxClCss_KeyIndex_t keyIdx, uint8_t const *pKey, size_t keyLength, size_t aadLength, size_t dataLength, uint8_t *pTag, uint8_t *pAeadCtx) |
| AES-GCM final encryption/decryption. More... | |
Defines all functions of mcuxClCss_Aead.
| MCUXCLCSS_API mcuxClCss_Status_Protected_t mcuxClCss_Aead_Init_Async | ( | mcuxClCss_AeadOption_t | options, |
| mcuxClCss_KeyIndex_t | keyIdx, | ||
| uint8_t const * | pKey, | ||
| size_t | keyLength, | ||
| uint8_t const * | pIV, | ||
| size_t | ivLength, | ||
| uint8_t * | pAeadCtx | ||
| ) |
AES-GCM initialization.
This is the first stage of AEAD encryption/decryption. This generates the initial context out of the IV pIV and the key (pKey or keyIdx).
Call mcuxClCss_WaitForOperation to complete the operation.
| [in] | options | The AEAD command options. For more information, see mcuxClCss_AeadOption_t. |
| [in] | keyIdx | Index of the key inside the CSSv2 keystore |
| [in] | pKey | Pointer to the key |
| [in] | keyLength | Size of pKey in bytes |
| [in] | pIV | Pointer to memory area that contains the IV |
| [in] | ivLength | Size of pIV in bytes, with padding |
| [out] | pAeadCtx | Pointer to the memory area that receives the AEAD context structure. Must be at least MCUXCLCSS_AEAD_CONTEXT_SIZE bytes long. |
The properties of some parameters change with respect to selected options.
options.extkey == MCUXCLCSS_AEAD_EXTERN_KEY keyIdx is ignored.
pKey must be a valid AES key and keyLength a valid AES key size (see MCUXCLCSS_CIPHER_KEY_SIZE_AES_).
options.extkey == MCUXCLCSS_AEAD_INTERN_KEY keyIdx must be a valid key index with the correct usage rights.
pKey and keyLength are ignored.
| MCUXCLCSS_STATUS_SW_INVALID_PARAM | if invalid parameters were specified |
| MCUXCLCSS_STATUS_SW_CANNOT_INTERRUPT | if a running operation prevented the request |
| MCUXCLCSS_STATUS_OK_WAIT | on successful request |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t mcuxClCss_Aead_PartialInit_Async | ( | mcuxClCss_AeadOption_t | options, |
| mcuxClCss_KeyIndex_t | keyIdx, | ||
| uint8_t const * | pKey, | ||
| size_t | keyLength, | ||
| uint8_t const * | pIV, | ||
| size_t | ivLength, | ||
| uint8_t * | pAeadCtx | ||
| ) |
AES-GCM partial initialization.
This is the first stage of AEAD encryption/decryption. This generates the initial context out of the IV pIV and the key (pKey or keyIdx).
Call mcuxClCss_WaitForOperation to complete the operation.
| [in] | options | The AEAD command options. For more information, see mcuxClCss_AeadOption_t. |
| [in] | keyIdx | Index of the key inside the CSSv2 keystore |
| [in] | pKey | Pointer to the key |
| [in] | keyLength | Size of pKey in bytes |
| [in] | pIV | Pointer to memory area that contains the IV |
| [in] | ivLength | Size of pIV in bytes, with padding |
| [out] | pAeadCtx | Pointer to the memory area that receives the AEAD context structure. Must be at least MCUXCLCSS_AEAD_CONTEXT_SIZE bytes long. |
The properties of some parameters change with respect to selected options.
options.extkey == MCUXCLCSS_AEAD_EXTERN_KEY keyIdx is ignored.
pKey must be a valid AES key and keyLength a valid AES key size (see MCUXCLCSS_CIPHER_KEY_SIZE_AES_).
options.extkey == MCUXCLCSS_AEAD_INTERN_KEY keyIdx must be a valid key index with the correct usage rights.
pKey and keyLength are ignored.
options.msgendw | MCUXCLCSS_STATUS_SW_INVALID_PARAM | if invalid parameters were specified |
| MCUXCLCSS_STATUS_SW_CANNOT_INTERRUPT | if a running operation prevented the request |
| MCUXCLCSS_STATUS_OK_WAIT | on successful request |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t mcuxClCss_Aead_UpdateAad_Async | ( | mcuxClCss_AeadOption_t | options, |
| mcuxClCss_KeyIndex_t | keyIdx, | ||
| uint8_t const * | pKey, | ||
| size_t | keyLength, | ||
| uint8_t const * | pAad, | ||
| size_t | aadLength, | ||
| uint8_t * | pAeadCtx | ||
| ) |
AES-GCM update of the Additional Authenticated Data (AAD)
This is the second stage of AEAD encryption/decryption. This updates the internal authentication tag with the AAD.
mcuxClCss_Aead_Init_Async must have been called before calling this function.
Call mcuxClCss_WaitForOperation to complete the operation.
| [in] | options | The AEAD command options. For more information, see mcuxClCss_AeadOption_t. |
| [in] | keyIdx | Index of the key inside the CSSv2 keystore |
| [in] | pKey | Pointer to the key |
| [in] | keyLength | Size of pKey in bytes |
| [in] | pAad | Memory area that contains the AAD |
| [in] | aadLength | Length of the pAad in bytes with padding |
| [in,out] | pAeadCtx | Pointer to the AEAD context structure. Must be at least MCUXCLCSS_AEAD_CONTEXT_SIZE bytes long. |
The properties of some parameters change with respect to selected options.
options.extkey == MCUXCLCSS_AEAD_EXTERN_KEY keyIdx is ignored.
pKey must be a valid AES key and keyLength a valid AES key size (see MCUXCLCSS_CIPHER_KEY_SIZE_AES_).
options.extkey == MCUXCLCSS_AEAD_INTERN_KEY keyIdx must be a valid key index with the correct usage rights.
pKey and keyLength are ignored.
options.msgendw | MCUXCLCSS_STATUS_SW_INVALID_PARAM | if invalid parameters were specified |
| MCUXCLCSS_STATUS_SW_CANNOT_INTERRUPT | if a running operation prevented the request |
| MCUXCLCSS_STATUS_OK_WAIT | on successful request |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t mcuxClCss_Aead_UpdateData_Async | ( | mcuxClCss_AeadOption_t | options, |
| mcuxClCss_KeyIndex_t | keyIdx, | ||
| uint8_t const * | pKey, | ||
| size_t | keyLength, | ||
| uint8_t const * | pInput, | ||
| size_t | inputLength, | ||
| uint8_t * | pOutput, | ||
| uint8_t * | pAeadCtx | ||
| ) |
AES-GCM update of the encrypted data.
This is the third stage of AEAD encryption/decryption. This updates the internal authentication tag with the AAD and outputs the ciphertext (in case of encryption) or plaintext (in case of decryption).
mcuxClCss_Aead_Init_Async, mcuxClCss_Aead_UpdateAad_Async must have been called before calling this function.
Call mcuxClCss_WaitForOperation to complete the operation.
| [in] | options | The AEAD command options. For more information, see mcuxClCss_AeadOption_t. |
| [in] | keyIdx | Index of the key inside the CSSv2 keystore |
| [in] | pKey | Pointer to the key |
| [in] | keyLength | Size of pKey in bytes |
| [in] | pInput | Pointer to the memory location of the data to be processed |
| [in] | inputLength | Size of pInput in bytes with padding |
| [out] | pOutput | Pointer to the processed data memory location |
| [in,out] | pAeadCtx | Pointer to the AEAD context structure. Must be at least MCUXCLCSS_AEAD_CONTEXT_SIZE bytes long. |
The properties of some parameters change with respect to selected options.
options.extkey == MCUXCLCSS_AEAD_EXTERN_KEY keyIdx is ignored.
pKey must be a valid AES key and keyLength a valid AES key size (see MCUXCLCSS_CIPHER_KEY_SIZE_AES_).
options.extkey == MCUXCLCSS_AEAD_INTERN_KEY keyIdx must be a valid key index with the correct usage rights.
pKey and keyLength are ignored.
options.msgendw | MCUXCLCSS_STATUS_SW_INVALID_PARAM | if invalid parameters were specified |
| MCUXCLCSS_STATUS_SW_CANNOT_INTERRUPT | if a running operation prevented the request |
| MCUXCLCSS_STATUS_OK_WAIT | on successful request |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t mcuxClCss_Aead_Finalize_Async | ( | mcuxClCss_AeadOption_t | options, |
| mcuxClCss_KeyIndex_t | keyIdx, | ||
| uint8_t const * | pKey, | ||
| size_t | keyLength, | ||
| size_t | aadLength, | ||
| size_t | dataLength, | ||
| uint8_t * | pTag, | ||
| uint8_t * | pAeadCtx | ||
| ) |
AES-GCM final encryption/decryption.
This is the fourth stage of AEAD encryption/decryption. This updates the authentication tag with the final data length block and outputs the tag at the desired location.
mcuxClCss_Aead_Init_Async, mcuxClCss_Aead_UpdateAad_Async and mcuxClCss_Aead_UpdateData_Async must have been called before calling this function.
Call mcuxClCss_WaitForOperation to complete the operation.
| [in] | options | The AEAD command options. For more information, see mcuxClCss_AeadOption_t. |
| [in] | keyIdx | Index of the key inside the CSSv2 keystore |
| [in] | pKey | Pointer to the key |
| [in] | keyLength | Size of pKey in bytes |
| [in] | aadLength | Length of the complete Additional Authenticated Data (AAD) in bytes, without padding. |
| [in] | dataLength | Length of the complete plaintext/ciphertext in bytes, without padding. |
| [out] | pTag | Pointer where the resulting tag will be stored |
| [in] | pAeadCtx | Pointer to the AEAD context structure. Must be at least MCUXCLCSS_AEAD_CONTEXT_SIZE bytes long. |
The properties of some parameters change with respect to selected options.
options.extkey == MCUXCLCSS_AEAD_EXTERN_KEY keyIdx is ignored.
pKey must be a valid AES key and keyLength a valid AES key size (see MCUXCLCSS_CIPHER_KEY_SIZE_AES_).
options.extkey == MCUXCLCSS_AEAD_INTERN_KEY keyIdx must be a valid key index with the correct usage rights.
pKey and keyLength are ignored.
options.msgendw | MCUXCLCSS_STATUS_SW_INVALID_PARAM | if invalid parameters were specified |
| MCUXCLCSS_STATUS_SW_CANNOT_INTERRUPT | if a running operation prevented the request |
| MCUXCLCSS_STATUS_OK_WAIT | on successful request |