Defines all functions of mcuxClCss_Cmac. More...
Functions | |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t | mcuxClCss_Cmac_Async (mcuxClCss_CmacOption_t options, mcuxClCss_KeyIndex_t keyIdx, uint8_t const *pKey, size_t keyLength, uint8_t const *pInput, size_t inputLength, uint8_t *pMac) |
| Performs CMAC with AES-128 or AES-256. More... | |
Defines all functions of mcuxClCss_Cmac.
| MCUXCLCSS_API mcuxClCss_Status_Protected_t mcuxClCss_Cmac_Async | ( | mcuxClCss_CmacOption_t | options, |
| mcuxClCss_KeyIndex_t | keyIdx, | ||
| uint8_t const * | pKey, | ||
| size_t | keyLength, | ||
| uint8_t const * | pInput, | ||
| size_t | inputLength, | ||
| uint8_t * | pMac | ||
| ) |
Performs CMAC with AES-128 or AES-256.
Call mcuxClCss_WaitForOperation to complete the operation.
| [in] | options | The command options. For more information, see mcuxClCss_CmacOption_t. |
| [in] | keyIdx | The CMAC key index |
| [in] | pKey | Pointer to the padded CMAC key |
| [in] | keyLength | Size of pKey in bytes. Must be a valid CMAC key size. See the parameter properties section in the function description. |
| [in] | pInput | Pointer to a memory location which contains the data, padded via SP 800-38b standard, to be authenticated |
| [in] | inputLength | Size of pInput in bytes before padding |
| [in,out] | pMac | Pointer to the CMAC command state input/output. See the parameter properties section in the function description. |
The properties of some parameters change with respect to selected options.
options.extkey == MCUXCLCSS_CMAC_EXTERNAL_KEY_ENABLE keyIdx is ignored.
options.extkey == MCUXCLCSS_CMAC_EXTERNAL_KEY_DISABLE pKey is ignored.
keyLength is ignored.
options.finalize == MCUXCLCSS_CMAC_FINALIZE_DISABLE) && (options.soe == MCUXCLCSS_CMAC_STATE_OUT_ENABLE) The intermediate state is written to pMac.
options.finalize == MCUXCLCSS_CMAC_FINALIZE_ENABLE The resulting MAC is written to pMac.
options.soe is ignored.
| MCUXCLCSS_STATUS_SW_INVALID_PARAM | if an invalid parameter was specified |
| MCUXCLCSS_STATUS_SW_CANNOT_INTERRUPT | if a running operation prevented the request |
| MCUXCLCSS_STATUS_OK_WAIT | on successful request |