Defines all functions of mcuxClCss_Hmac. More...
Functions | |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t | mcuxClCss_Hmac_Async (mcuxClCss_HmacOption_t options, mcuxClCss_KeyIndex_t keyIdx, uint8_t const *pPaddedKey, uint8_t const *pInput, size_t inputLength, uint8_t *pOutput) |
| Performs HMAC with SHA-256. More... | |
Defines all functions of mcuxClCss_Hmac.
| MCUXCLCSS_API mcuxClCss_Status_Protected_t mcuxClCss_Hmac_Async | ( | mcuxClCss_HmacOption_t | options, |
| mcuxClCss_KeyIndex_t | keyIdx, | ||
| uint8_t const * | pPaddedKey, | ||
| uint8_t const * | pInput, | ||
| size_t | inputLength, | ||
| uint8_t * | pOutput | ||
| ) |
Performs HMAC with SHA-256.
Call mcuxClCss_WaitForOperation to complete the operation.
| [in] | options | The command options. For more information, see mcuxClCss_HmacOption_t. |
| [in] | keyIdx | The HMAC key index, if an internal key shall be used |
| [in] | pPaddedKey | Pointer to a memory location containing the padded HMAC key |
| [in] | pInput | Pointer to a memory location which contains the data to be authenticated |
| [in] | inputLength | Size of pInput in bytes |
| [out] | pOutput | The output message authentication code |
The properties of some parameters change with respect to selected options.
options.extkey == MCUXCLCSS_HMAC_EXTERNAL_KEY_ENABLE keyIdx is ignored.
pPaddedKey must contain the padded HMAC key, which can mean one of two things depending on the length of the original HMAC key, LkHMAC:
If LkHMAC ≤ MCUXCLCSS_HMAC_PADDED_KEY_SIZE, pPaddedKey must be the HMAC key padded with zero-bytes to fill the required length of MCUXCLCSS_HMAC_PADDED_KEY_SIZE bytes.
pPaddedKey must contain the SHA-256 hash of the HMAC key, padded with zero-bytes to fill the required length of MCUXCLCSS_HMAC_PADDED_KEY_SIZE bytes.options.extkey == MCUXCLCSS_HMAC_EXTERNAL_KEY_DISABLE keyIdx must be a valid key index with the correct usage rights for HMAC.
pPaddedKey is ignored.
| MCUXCLCSS_STATUS_SW_INVALID_PARAM | if an invalid parameter was specified |
| MCUXCLCSS_STATUS_SW_CANNOT_INTERRUPT | if a running operation prevented the request |
| MCUXCLCSS_STATUS_OK_WAIT | on successful request |