Defines all functions of mcuxClCss_Kdf.
More...
|
| MCUXCLCSS_API mcuxClCss_Status_Protected_t | mcuxClCss_Hkdf_Rfc5869_Async (mcuxClCss_HkdfOption_t options, mcuxClCss_KeyIndex_t derivationKeyIdx, mcuxClCss_KeyIndex_t targetKeyIdx, mcuxClCss_KeyProp_t targetKeyProperties, uint8_t const *pDerivationData) |
| | Derives a key using the HKDF (HMAC-based key derivation function) according to RFC5869. More...
|
| |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t | mcuxClCss_Hkdf_Sp80056c_Async (mcuxClCss_KeyIndex_t derivationKeyIdx, uint8_t *pTagetKey, uint8_t const *pDerivationData, size_t derivationDataLength) |
| | Derives a key using the HKDF (HMAC-based key derivation function) according to SP800-56C one-step approach with Sha2-256. More...
|
| |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t | mcuxClCss_Ckdf_Sp800108_Async (mcuxClCss_KeyIndex_t derivationKeyIdx, mcuxClCss_KeyIndex_t targetKeyIdx, mcuxClCss_KeyProp_t targetKeyProperties, uint8_t const *pDerivationData) |
| | Derives a key using the NIST SP 800-108 CMAC-based Extract-and-Expand Key Derivation Function. More...
|
| |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t | mcuxClCss_TlsGenerateMasterKeyFromPreMasterKey_Async (uint8_t const *pDerivationData, mcuxClCss_KeyProp_t keyProperties, mcuxClCss_KeyIndex_t keyIdx) |
| | Generates a TLS master key based on a pre-master key and derivation data, according to the TLS 1.2 specification. More...
|
| |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t | mcuxClCss_TlsGenerateSessionKeysFromMasterKey_Async (uint8_t const *pDerivationData, mcuxClCss_KeyProp_t keyProperties, mcuxClCss_KeyIndex_t keyIdx) |
| | Generates TLS session keys based on a master key and derivation data, according to the TLS 1.2 specification. More...
|
| |
Defines all functions of mcuxClCss_Kdf.
◆ mcuxClCss_Hkdf_Rfc5869_Async()
Derives a key using the HKDF (HMAC-based key derivation function) according to RFC5869.
Call mcuxClCss_WaitForOperation to complete the operation.
- Parameters
-
| [in] | options | The command options. For more information, see mcuxClCss_HkdfOption_t. |
| [in] | derivationKeyIdx | Key index used for derivation. Must be a 256-bit key with HKDF property bit set to 1. |
| [in] | targetKeyIdx | Key bank number of the derived key. Will be a 256-bit key, the user must ensure there is enough space in the keystore to hold the derived key. |
| [in] | targetKeyProperties | Requested properties for the derived key. The ksize field will be ignored. |
| [in] | pDerivationData | The algorithm-specific derivation data, the length is MCUXCLCSS_HKDF_RFC5869_DERIVATIONDATA_SIZE bytes |
- Returns
- An error code that can be any error code in MCUXCLCSS_STATUS_, see individual documentation for more information
- Return values
-
◆ mcuxClCss_Hkdf_Sp80056c_Async()
Derives a key using the HKDF (HMAC-based key derivation function) according to SP800-56C one-step approach with Sha2-256.
Call mcuxClCss_WaitForOperation to complete the operation.
- Parameters
-
| [in] | derivationKeyIdx | Key index used for derivation. Must be a 256-bit key with HKDF property bit set to 1. |
| [out] | pTagetKey | Memory area to store the derived key. Will be a 256-bit key, the user must ensure there is enough space in the keystore to hold the derived key. |
| [in] | pDerivationData | The algorithm-specific derivation data |
| [in] | derivationDataLength | Length of the derivation data |
- Returns
- An error code that can be any error code in MCUXCLCSS_STATUS_, see individual documentation for more information
- Return values
-
◆ mcuxClCss_Ckdf_Sp800108_Async()
Derives a key using the NIST SP 800-108 CMAC-based Extract-and-Expand Key Derivation Function.
Call mcuxClCss_WaitForOperation to complete the operation.
- Parameters
-
| [in] | derivationKeyIdx | Key index used for derivation |
| [in] | targetKeyIdx | Key bank number of the derived key |
| [in] | targetKeyProperties | Requested properties for the derived key. Only set usage bits. |
| [in] | pDerivationData | The algorithm-specific derivation data, the length is MCUXCLCSS_CKDF_DERIVATIONDATA_SIZE bytes |
- Returns
- An error code that can be any error code in MCUXCLCSS_STATUS_, see individual documentation for more information
- Return values
-
◆ mcuxClCss_TlsGenerateMasterKeyFromPreMasterKey_Async()
Generates a TLS master key based on a pre-master key and derivation data, according to the TLS 1.2 specification.
The pre-master key is overwritten in this operation. Call mcuxClCss_WaitForOperation to complete the operation.
- Parameters
-
- Returns
- An error code that can be any error code in MCUXCLCSS_STATUS_, see individual documentation for more information
- Return values
-
- Examples
- tls_master_key_session_keys.c.
◆ mcuxClCss_TlsGenerateSessionKeysFromMasterKey_Async()
Generates TLS session keys based on a master key and derivation data, according to the TLS 1.2 specification.
The master key and the following five key indices are overwritten in this operation. The keys are written in the following order:
-
Client Encryption Key
-
Client Message Authentication Key
-
Server Encryption Key
-
Server Message Authentication Key
Call mcuxClCss_WaitForOperation to complete the operation.
- Parameters
-
- Returns
- An error code that can be any error code in MCUXCLCSS_STATUS_, see individual documentation for more information
- Return values
-
- Examples
- tls_master_key_session_keys.c.