Defines all functions of mcuxClCss_KeyManagement. More...
Functions | |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t | mcuxClCss_KeyDelete_Async (mcuxClCss_KeyIndex_t keyIdx) |
| Deletes a key from keystore at the given index. More... | |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t | mcuxClCss_KeyImport_Async (mcuxClCss_KeyImportOption_t options, uint8_t const *pImportKey, size_t importKeyLength, mcuxClCss_KeyIndex_t wrappingKeyIdx, mcuxClCss_KeyIndex_t targetKeyIdx) |
| Imports a key from external storage to an internal key register. More... | |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t | mcuxClCss_KeyExport_Async (mcuxClCss_KeyIndex_t wrappingKeyIdx, mcuxClCss_KeyIndex_t exportKeyIdx, uint8_t *pOutput) |
| Exports a key from an internal key register to external storage, using a wrapping key. More... | |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t | mcuxClCss_GetKeyProperties (mcuxClCss_KeyIndex_t keyIdx, mcuxClCss_KeyProp_t *pKeyProp) |
| Exports the properties of the keys stored in the CSS internal keystore. More... | |
Defines all functions of mcuxClCss_KeyManagement.
| MCUXCLCSS_API mcuxClCss_Status_Protected_t mcuxClCss_KeyDelete_Async | ( | mcuxClCss_KeyIndex_t | keyIdx | ) |
Deletes a key from keystore at the given index.
Before execution, CSS will wait until mcuxClCss_HwState_t.drbgentlvl == MCUXCLCSS_STATUS_DRBGENTLVL_LOW. This can lead to a delay if the DRBG is in a state with less security strength at the time of the call.
Call mcuxClCss_WaitForOperation to complete the operation.
| [in] | keyIdx | The index of the key to be deleted |
| MCUXCLCSS_STATUS_SW_INVALID_PARAM | if invalid parameters were specified |
| MCUXCLCSS_STATUS_SW_CANNOT_INTERRUPT | if a running operation prevented the request |
| MCUXCLCSS_STATUS_OK_WAIT | on successful request |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t mcuxClCss_KeyImport_Async | ( | mcuxClCss_KeyImportOption_t | options, |
| uint8_t const * | pImportKey, | ||
| size_t | importKeyLength, | ||
| mcuxClCss_KeyIndex_t | wrappingKeyIdx, | ||
| mcuxClCss_KeyIndex_t | targetKeyIdx | ||
| ) |
Imports a key from external storage to an internal key register.
Call mcuxClCss_WaitForOperation to complete the operation.
| [in] | options | One of MCUXCLCSS_KEYIMPORT_KFMT_ |
| [in] | pImportKey | Pointer to the RFC3394 container of the key to be imported |
| [in] | importKeyLength | Length of the RFC3394 container of the key to be imported |
| [in] | wrappingKeyIdx | Index of the key wrapping key, if importing RFC3394 format |
| [in] | targetKeyIdx | The desired key index of the imported key |
options.kfmt != MCUXCLCSS_KEYIMPORT_KFMT_RFC3394pImportKey is ignored. importKeyLength is ignored. wrappingKeyIdx is ignored. targetKeyIdx is ignored. The unpacked key is automatically stored in key slots 0, 1. | MCUXCLCSS_STATUS_SW_INVALID_PARAM | if invalid parameters were specified |
| MCUXCLCSS_STATUS_SW_CANNOT_INTERRUPT | if a running operation prevented the request |
| MCUXCLCSS_STATUS_OK_WAIT | on successful request |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t mcuxClCss_KeyExport_Async | ( | mcuxClCss_KeyIndex_t | wrappingKeyIdx, |
| mcuxClCss_KeyIndex_t | exportKeyIdx, | ||
| uint8_t * | pOutput | ||
| ) |
Exports a key from an internal key register to external storage, using a wrapping key.
Call mcuxClCss_WaitForOperation to complete the operation.
| [in] | wrappingKeyIdx | The key used for key wrapping |
| [in] | exportKeyIdx | The key to export |
| [out] | pOutput | The memory address of the exported key |
| MCUXCLCSS_STATUS_SW_INVALID_PARAM | if invalid parameters were specified |
| MCUXCLCSS_STATUS_SW_CANNOT_INTERRUPT | if a running operation prevented the request |
| MCUXCLCSS_STATUS_OK_WAIT | on successful request |
| [in] | wrappingKeyIdx | The key used for key wrapping |
| [in] | exportKeyIdx | The key to export |
| [out] | pOutput | The memory address of the exported key |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t mcuxClCss_GetKeyProperties | ( | mcuxClCss_KeyIndex_t | keyIdx, |
| mcuxClCss_KeyProp_t * | pKeyProp | ||
| ) |
Exports the properties of the keys stored in the CSS internal keystore.
Call mcuxClCss_WaitForOperation to complete the operation.
| [in] | keyIdx | Request key properties of the index defined here |
| [out] | pKeyProp | Key properties of the index provided |
| MCUXCLCSS_STATUS_SW_CANNOT_INTERRUPT | if a running operation prevented the request |
| MCUXCLCSS_STATUS_OK | on successful request |