Defines all macros of mcuxClCss_Types. More...
Modules | |
| MCUXCLCSS_KEYPROPERTY_VALUE_ | |
| Constants for initalizing mcuxClCss_KeyProp_t.word. | |
| MCUXCLCSS_KEYPROPERTY_ | |
| Constants for initalizing mcuxClCss_KeyProp_t.bits. | |
| MCUXCLCSS_STATUS_ | |
| Return code definitions. | |
Macros | |
| #define | MCUXCLCSS_KEY_SLOTS |
| Number of key slots in the CSS key store. More... | |
| #define | MCUXCLCSS_STATUS_IS_HW_ERROR(x) |
| Checks whether an error code is a hardware error. Indicates that an error was reported by CSSv2 hardware. More... | |
| #define | MCUXCLCSS_STATUS_IS_SW_ERROR(x) |
| Checks whether an error code is a software error. Indicates that the error was detected by the driver software and not by CSSv2 hardware. More... | |
Defines all macros of mcuxClCss_Types.
| #define MCUXCLCSS_KEY_SLOTS |
Number of key slots in the CSS key store.
| #define MCUXCLCSS_STATUS_IS_HW_ERROR | ( | x | ) |
Checks whether an error code is a hardware error. Indicates that an error was reported by CSSv2 hardware.
| #define MCUXCLCSS_STATUS_IS_SW_ERROR | ( | x | ) |
Checks whether an error code is a software error. Indicates that the error was detected by the driver software and not by CSSv2 hardware.