Defines all functions of mcuxClHash. More...
Functions | |
| mcuxClHash_Status_Protected_t | mcuxClHash_compute (mcuxClSession_Handle_t session, const mcuxClHash_Algo_t *algo, const uint8_t *const in, uint32_t inSize, uint8_t *const hash, uint8_t *const rtf) |
| One-shot hash computation. More... | |
| mcuxClHash_Status_Protected_t | mcuxClHash_init (mcuxClSession_Handle_t session, mcuxClHash_Context_t *context, const mcuxClHash_Algo_t *algo) |
| Initializes the context for a new hash computation. More... | |
| mcuxClHash_Status_Protected_t | mcuxClHash_update (mcuxClSession_Handle_t session, mcuxClHash_Context_t *context, const uint8_t *const in, uint32_t inSize) |
| Adds a chunk of data to an ongoing hash computation. More... | |
| mcuxClHash_Status_Protected_t | mcuxClHash_finish (mcuxClSession_Handle_t session, mcuxClHash_Context_t *context, uint8_t *const hash, uint8_t *const rtf) |
| Finishes a hash computation. More... | |
Defines all functions of mcuxClHash.
| mcuxClHash_Status_Protected_t mcuxClHash_compute | ( | mcuxClSession_Handle_t | session, |
| const mcuxClHash_Algo_t * | algo, | ||
| const uint8_t *const | in, | ||
| uint32_t | inSize, | ||
| uint8_t *const | hash, | ||
| uint8_t *const | rtf | ||
| ) |
One-shot hash computation.
This function computes the hash over the input message in using the hash function provided by the algo input parameter.
The input parameter session has to be initialized by the function mcuxClSession_init prior to calling this function. Certain mcuxClHashAlgorithms support maintaining a Runtime Fingerprint (RTF). Updating of the RTF has to be enabled/disabled by calling the mcuxClSession_setRtf function on the session prior to calling this function.
| session | Session to be used with the hash function. |
| algo | Algorithm to be used with the hash function. |
| in | Pointer to the input message |
| inSize | Length of the input message |
| hash | Computed hash value over the input message |
| rtf | Updated RTF value after the hash operation. Only supported on platforms with CSS (Platform specific) |
| MCUXCLHASH_STATUS_OK | Hash operation successful |
| MCUXCLHASH_STATUS_ERROR | Error occured during Hash operation |
| mcuxClHash_Status_Protected_t mcuxClHash_init | ( | mcuxClSession_Handle_t | session, |
| mcuxClHash_Context_t * | context, | ||
| const mcuxClHash_Algo_t * | algo | ||
| ) |
Initializes the context for a new hash computation.
The function initializes the context for the selected hash algorithm.
Up to 2^32 bytes of data can be hashed with a single context.
| session | Session to be used with the hash function. |
| context | The context to initialize. |
| algo | The selected hashing algorithm. This parameter must point to a statically allocated object (static or global variable). |
| MCUXCLHASH_STATUS_OK | Hash operation successful |
| MCUXCLHASH_STATUS_ERROR | Error occured during Hash operation |
| mcuxClHash_Status_Protected_t mcuxClHash_update | ( | mcuxClSession_Handle_t | session, |
| mcuxClHash_Context_t * | context, | ||
| const uint8_t *const | in, | ||
| uint32_t | inSize | ||
| ) |
Adds a chunk of data to an ongoing hash computation.
This function appends the additional data to the context.
Up to 2^32 bytes of data can be hashed with a single context.
| session | Session to be used with the hash function. |
| context | The hash context. |
| in | Pointer to the data to be added to the hash. |
| inSize | Size of the data to be added to the hash. |
| MCUXCLHASH_STATUS_OK | Hash operation successful |
| MCUXCLHASH_STATUS_ERROR | Error occured during Hash operation |
| mcuxClHash_Status_Protected_t mcuxClHash_finish | ( | mcuxClSession_Handle_t | session, |
| mcuxClHash_Context_t * | context, | ||
| uint8_t *const | hash, | ||
| uint8_t *const | rtf | ||
| ) |
Finishes a hash computation.
This function processes the padding and outputs the resulting hash to the given buffer.
| session | Session to be used with the hash function. |
| context | The hash context. |
| hash | Pointer to the location where the function should write the resulting hash. |
| rtf | Pointer to the location where the function should write the run-time fingerprint (RTF). Only supported on platforms with CSSv2. If RTF updates are not enabled in the session, this pointer may be NULL. |
| MCUXCLHASH_STATUS_OK | Hash operation successful |
| MCUXCLHASH_STATUS_ERROR | Error occured during Hash operation |