Defines all functions of mcuxClKey.
More...
|
| mcuxClKey_Status_Protected_t | mcuxClKey_init (mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, const mcuxClKey_Type_t *type, const mcuxClKey_Protection_t *protection, const uint8_t *const srcKeyData, const uint8_t *const srcAuxData, uint32_t srcAuxSlot) |
| | Initializes a key handle. More...
|
| |
| mcuxClKey_Status_Protected_t | mcuxClKey_loadCopro (mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, uint32_t dstSlot) |
| | Load key into destination key slot of a coprocessor. More...
|
| |
| mcuxClKey_Status_Protected_t | mcuxClKey_loadMemory (mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, uint32_t *dstData) |
| | Load key into destination memory buffer. More...
|
| |
| mcuxClKey_Status_Protected_t | mcuxClKey_flush (mcuxClSession_Handle_t session, mcuxClKey_Handle_t key) |
| | Flush key from destination which can be a key slot of coprocessor or memory buffer. More...
|
| |
| mcuxClKey_Status_Protected_t | mcuxClKey_setKeyproperties (mcuxClKey_Handle_t key, mcuxClCss_KeyProp_t key_properties) |
| | Set the requested key properties of the destination key. More...
|
| |
Defines all functions of mcuxClKey.
◆ mcuxClKey_init()
Initializes a key handle.
- Parameters
-
| [in] | session | Session handle to provide session dependent information |
| [in,out] | key | Key handle that will be initialized |
| [in] | type | Define which key type shall be initialized |
| [in] | protection | Define the protection and flush mechanism that shall be initialized |
| [in] | srcKeyData | Provide pointer to source data of the key. This can be a pointer to a plain key buffer, a share, or a key blob. The protection function defines the purpose of this parameter |
| [in] | srcAuxData | Provide pointer to aux data of the key. This can be a pointer to a a share, or a wrapping key, or derivation data. The protection function defines the purpose of this parameter |
| [in] | srcAuxSlot | Provide aux key slot in case the key is present in a coprocessor keyslot. The protection function defines the purpose of this parameter |
- Returns
- An error code that can be any error code in MCUXCLKEY_STATUS_, see individual documentation for more information
- Return values
-
- Examples
- mcuxClKey_example.c, and mcuxClMac_cmac_oneshot_example.c.
◆ mcuxClKey_loadCopro()
Load key into destination key slot of a coprocessor.
- Parameters
-
| [in] | session | Session handle to provide session dependent information |
| [in] | key | Key handle that provides information to load the key |
| [out] | dstSlot | Provide destination key slot in case the key has to loaded to a key slot. The protection function defines the purpose of this parameter |
- Returns
- An error code that can be any error code in MCUXCLKEY_STATUS_, see individual documentation for more information
- Return values
-
◆ mcuxClKey_loadMemory()
Load key into destination memory buffer.
- Parameters
-
| [in] | session | Session handle to provide session dependent information |
| [in] | key | Key handle that provides information to load the key |
| [out] | dstData | Provide pointer to destination key memory in case the key has to be loaded to memory. The protection function defines the purpose of this parameter |
- Returns
- An error code that can be any error code in MCUXCLKEY_STATUS_, see individual documentation for more information
- Return values
-
- Examples
- mcuxClKey_example.c, and mcuxClMac_cmac_oneshot_example.c.
◆ mcuxClKey_flush()
Flush key from destination which can be a key slot of coprocessor or memory buffer.
- Parameters
-
| [in] | session | Session handle to provide session dependent information |
| [in] | key | Key handle that provides information to flush the key |
- Returns
- An error code that can be any error code in MCUXCLKEY_STATUS_, see individual documentation for more information
- Return values
-
- Examples
- mcuxClKey_example.c, and mcuxClMac_cmac_oneshot_example.c.
◆ mcuxClKey_setKeyproperties()
Set the requested key properties of the destination key.
- Parameters
-
| [in,out] | key | key handle that provides information to flush the key |
| [in] | key_properties | Set requested key properties of the destination key |
- Returns
- An error code that can be any error code in MCUXCLKEY_STATUS_, see individual documentation for more information
- Return values
-
- Examples
- mcuxClKey_example.c, and mcuxClMac_cmac_oneshot_example.c.
◆ mcuxClKey_protection_none
◆ mcuxClKey_protection_ckdf
Protection function pointer for CSS internal CKDF based key generation.
See mcuxClKey_Protection for the structure definition. Initializing mcuxClKey_Handle_t with this pointer (via mcuxClKey_init) to use CSS internal CKDF based key generation.
- Parameters defined by protection function
- mcuxClKey_init
- srcKeyData
- RFU.
- srcAuxData
- Pointer to key derivation data.
- srcAuxSlot
- Master key slot.
- mcuxClKey_loadCopro
- dstSlot
- Destination key slot of key.
- mcuxClKey_loadMemory
- This function shall not be used by this protection mechanism.