Defines all types of the mcuxClMac component. More...
Macros | |
| #define | MCUXCLMAC_ERRORCODE_OK |
| Mac operation successful. More... | |
| #define | MCUXCLMAC_ERRORCODE_ERROR |
| Error occurred during Mac operation. More... | |
| #define | MCUXCLMAC_ERRORCODE_FAULT_ATTACK |
| Fault attack (unexpected behaviour) detected. More... | |
| #define | MCUXCL_HMAC_SIZE_OF_LENGTH_FIELD |
| Size of HMAC length field. More... | |
| #define | MCUXCL_HMAC_MIN_PADDING_LENGTH |
| Size of minimum HMAC padding length. More... | |
| #define | MCUXCLMAC_GET_HMAC_INPUTBUFFER_LENGTH(dataLength) |
| Formula to calculate input buffer size for HMAC with SHA-256. More... | |
Typedefs | |
| typedef uint32_t | mcuxClMac_Status_t |
| Type for Mac component error codes. More... | |
| typedef uint64_t | mcuxClMac_Status_Protected_t |
| Type for error codes used by code-flow protected Mac component functions. More... | |
| typedef struct mcuxClMac_Mode | mcuxClMac_Mode_t |
| Mac Mode type. More... | |
| typedef struct mcuxClMac_Context | mcuxClMac_Context_t |
| Mac context type. More... | |
| typedef struct mcuxClMac_WaCpu_t | mcuxClMac_WaCpu_t |
| Mac Cpu Work Area type. More... | |
Variables | |
| const mcuxClMac_Mode_t | mcuxClMac_Mode_CMAC |
| Mode definition for CMAC. More... | |
| const mcuxClMac_Mode_t | mcuxClMac_Mode_HMAC_SHA2_256 |
| Mode definition for HMAC_SHA2_256. More... | |
Defines all types of the mcuxClMac component.
| #define MCUXCLMAC_ERRORCODE_OK |
Mac operation successful.
| #define MCUXCLMAC_ERRORCODE_ERROR |
Error occurred during Mac operation.
| #define MCUXCLMAC_ERRORCODE_FAULT_ATTACK |
Fault attack (unexpected behaviour) detected.
| #define MCUXCL_HMAC_SIZE_OF_LENGTH_FIELD |
Size of HMAC length field.
| #define MCUXCL_HMAC_MIN_PADDING_LENGTH |
Size of minimum HMAC padding length.
| #define MCUXCLMAC_GET_HMAC_INPUTBUFFER_LENGTH | ( | dataLength | ) |
Formula to calculate input buffer size for HMAC with SHA-256.
| typedef uint32_t mcuxClMac_Status_t |
Type for Mac component error codes.
| typedef uint64_t mcuxClMac_Status_Protected_t |
Type for error codes used by code-flow protected Mac component functions.
| typedef struct mcuxClMac_Mode mcuxClMac_Mode_t |
Mac Mode type.
This internal type provides all implementation details for a mode to the top level mcuxClMac functions
| typedef struct mcuxClMac_Context mcuxClMac_Context_t |
Mac context type.
This type captures all the information that the Mac interface needs to know for a particular Mac mode/algorithm to work.
The size of the context depends on the mode used (see mcuxClMac_MemoryConsumption).
| typedef struct mcuxClMac_WaCpu_t mcuxClMac_WaCpu_t |
Mac Cpu Work Area type.
| const mcuxClMac_Mode_t mcuxClMac_Mode_CMAC |
Mode definition for CMAC.
| const mcuxClMac_Mode_t mcuxClMac_Mode_HMAC_SHA2_256 |
Mode definition for HMAC_SHA2_256.
HMAC_SHA2_256 can only be executed in Oneshot mode. Partial processing is not supported.
The input buffer will be modified by applying padding to it. The caller must ensure that the input buffer is large enough by determining its size using MCUXCLMAC_GET_HMAC_INPUTBUFFER_LENGTH on the input.
Also note that HMAC only works with keys loaded into coprocessor (see mcuxClKey for details).