This function clears a memory region. More...
Functions | |
| mcuxClMemory_Status_Protected_t | mcuxClMemory_clear (uint8_t *dst, size_t len, size_t buflen) |
| Overwrites a memory buffer with null bytes. More... | |
This function clears a memory region.
| mcuxClMemory_Status_Protected_t mcuxClMemory_clear | ( | uint8_t * | dst, |
| size_t | len, | ||
| size_t | buflen | ||
| ) |
Overwrites a memory buffer with null bytes.
| [out] | dst | Pointer to the buffer to be cleared. |
| [in] | len | size (in bytes) to be cleared. |
| [in] | buflen | buffer size (if buflen < len, only buflen bytes are cleared). |