This function sets all bytes in a memory region to a specified value. More...
Functions | |
| mcuxClMemory_Status_Protected_t | mcuxClMemory_set (uint8_t *dst, uint8_t val, size_t len, size_t buflen) |
| Sets all bytes of a memory buffer to a specified value. More... | |
This function sets all bytes in a memory region to a specified value.
| mcuxClMemory_Status_Protected_t mcuxClMemory_set | ( | uint8_t * | dst, |
| uint8_t | val, | ||
| size_t | len, | ||
| size_t | buflen | ||
| ) |
Sets all bytes of a memory buffer to a specified value.
| [out] | dst | pointer to the buffer to be set. |
| [in] | val | byte value to be set. |
| [in] | len | size (in bytes) to be set. |
| [in] | buflen | buffer size (if buflen < len, only buflen bytes are set). |