mcuxClPkc functions of PKC calculation
More...
mcuxClPkc functions of PKC calculation
◆ MCUXCLPKC_FP_CALCFUP
| #define MCUXCLPKC_FP_CALCFUP |
( |
|
pUPTR, |
|
|
|
ulen |
|
) |
| |
◆ MCUXCLPKC_FP_CALCFUP_OFFSET
| #define MCUXCLPKC_FP_CALCFUP_OFFSET |
( |
|
pUPTR, |
|
|
|
skipLen, |
|
|
|
ulen |
|
) |
| |
Helper macro to call mcuxClPkc_CalcFup (skipping first skipLen calculation(s)) with flow protection.
◆ mcuxClPkc_PtrFUPEntry_t
type of FUP program address.
◆ mcuxClPkc_Calc()
Start a PKC calculation.
This function performs one specified PKC calculation, of which the operand(s) and result are specified by the indices of UPTR table.
- Parameters
-
| [in] | param_mode | param (the higher 8 bits) indicates the type of the calculation (L0 or L1) and the parameter set (PS1 or PS2).
mode (the lower 8 bits) indicates the calculation, either an L0 operation or L1 microcode. |
| [in] | iR_iX_iY_iZ | indices of the operand(s) and the result in UPTR table. |
- Returns
- A flow-protected status code (see Flow Protection API).
- Return values
-
- Attention
- The PKC calculation might be still on-going, call mcuxClPkc_WaitForFinish before CPU accesses to the result.
◆ mcuxClPkc_CalcConst()
Start a PKC calculation with one constant parameter.
This function performs one specified PKC calculation, of which the operand(s) and result are specified by the indices of UPTR table, and a 8-bit constant parameter is directly provided.
- Parameters
-
| [in] | param_mode | param (the higher 8 bits) indicates the type of the calculation (always L0) and the parameter set (PS1 or PS2).
mode (the lower 8 bits) indicates the calculation, an L0 operation. |
| [in] | iR_iX_iY_C | indices of the operand(s) and the result in UPTR table, and a direct 8-bit constant. |
- Returns
- A flow-protected status code (see Flow Protection API).
- Return values
-
- Attention
- The PKC calculation might be still on-going, call mcuxClPkc_WaitForFinish before CPU accesses to the result.
◆ mcuxClPkc_CalcFup()
Start a PKC FUP program calculation.
This function triggers PKC to start the calculation of a FUP program.
- Parameters
-
| [in] | pUPTR | address of the FUP program. |
| [in] | ulen | length (number of calculation) of the FUP program. |
- Returns
- A flow-protected status code (see Flow Protection API).
- Return values
-
- Attention
- The PKC calculation might be still on-going, call mcuxClPkc_WaitForFinish before CPU accesses to the result.