mcuxCsslMemory_Clear Function Definitions More...
Functions | |
| mcuxCsslMemory_ClearResult_t | mcuxCsslMemory_Clear (mcuxCsslParamIntegrity_Checksum_t chk, void *pDst, size_t dst_size, size_t cnt) |
Clear cnt bytes of data at pDst. More... | |
mcuxCsslMemory_Clear Function Definitions
| mcuxCsslMemory_ClearResult_t mcuxCsslMemory_Clear | ( | mcuxCsslParamIntegrity_Checksum_t | chk, |
| void * | pDst, | ||
| size_t | dst_size, | ||
| size_t | cnt | ||
| ) |
Clear cnt bytes of data at pDst.
The implementation is secure in the following aspects: Parameter integrity protection: the function returns immediately in case of an incorrect parameter checksum. Code flow protection: the function call is protected. Buffer overflow protection: no data is written to pDst beyond dst_size bytes.
| [in] | chk | The parameter checksum, generated with mcuxCsslParamIntegrity_Protect. |
| [in] | pDst | The destination pointer to buffer to be cleared. Must not be NULL. |
| [in] | dst_size | The size of the destination data buffer in bytes. |
| [in] | cnt | The number of bytes to clear. Must be different from zero. |
| MCUXCSSLMEMORY_CLEAR_SUCCESS | If the contents in buffer at pDst is cleared. |
| MCUXCSSLMEMORY_CLEAR_INVALID_PARAMETER | If one of the parameters is invalid. |
| MCUXCSSLMEMORY_CLEAR_FAULT | If a fault was detected, included invalid checksum chk. |