Macros of mcuxCsslParamIntegrity component. More...
Macros | |
| #define | MCUXCSSLPARAMINTEGRITY_BASE_CHECKSUM |
| First eight hex digits of Euler's number. More... | |
| #define | MCUXCSSLPARAMINTEGRITY_CHECK_VALID |
| Return value of mcuxCsslParamIntegrity_Validate if the parameter checksum was correct. More... | |
| #define | MCUXCSSLPARAMINTEGRITY_CHECK_INVALID |
| Return value of mcuxCsslParamIntegrity_Validate if the parameter checksum was incorrect. More... | |
Macros of mcuxCsslParamIntegrity component.
| #define MCUXCSSLPARAMINTEGRITY_BASE_CHECKSUM |
First eight hex digits of Euler's number.
| #define MCUXCSSLPARAMINTEGRITY_CHECK_VALID |
Return value of mcuxCsslParamIntegrity_Validate if the parameter checksum was correct.
| #define MCUXCSSLPARAMINTEGRITY_CHECK_INVALID |
Return value of mcuxCsslParamIntegrity_Validate if the parameter checksum was incorrect.