Example of SHA2-384 hashing using the CSSv2 (CLNS component mcuxClCss) More...
Functions | |
| bool | hash_sha384_one_block (void) |
| Performs SHA2-384 hashing using mcuxClCss functions. More... | |
Variables | |
| static uint8_t const | sha384_padded_input [MCUXCLCSS_HASH_BLOCK_SIZE_SHA_384] |
| Data input for SHA2-384 hashing. More... | |
| static uint8_t | sha384_reference_digest [MCUXCLCSS_HASH_OUTPUT_SIZE_SHA_384] |
| Expected hash value. More... | |
| static uint8_t | sha2_384_digest [MCUXCLCSS_HASH_STATE_SIZE_SHA_384] |
| Destination buffer to receive the hash output of the SHA2-384 hashing. More... | |
Example of SHA2-384 hashing using the CSSv2 (CLNS component mcuxClCss)
| bool hash_sha384_one_block | ( | void | ) |
Performs SHA2-384 hashing using mcuxClCss functions.
| true | The example code completed successfully |
| false | The example code failed |
|
static |
Data input for SHA2-384 hashing.
|
static |
Expected hash value.
|
static |
Destination buffer to receive the hash output of the SHA2-384 hashing.