CSSv2 header for symmetric ciphers. More...
#include <mcuxClCss_Common.h>Go to the source code of this file.
Data Structures | |
| union | mcuxClCss_CipherOption_t |
| Command option bit field for mcuxClCss_Cipher_Async. More... | |
Macros | |
| #define | MCUXCLCSS_CIPHER_ENCRYPT |
| Set this option at mcuxClCss_CipherOption_t.dcrpt to perform an encryption. More... | |
| #define | MCUXCLCSS_CIPHER_DECRYPT |
| Set this option at mcuxClCss_CipherOption_t.dcrpt to perform a decryption. More... | |
| #define | MCUXCLCSS_CIPHER_STATE_OUT_ENABLE |
Set this option at mcuxClCss_CipherOption_t.cphsoe to export the internal CSS state to pIV. More... | |
| #define | MCUXCLCSS_CIPHER_STATE_OUT_DISABLE |
| Set this option at mcuxClCss_CipherOption_t.cphsoe to not export the internal CSS state. More... | |
| #define | MCUXCLCSS_CIPHER_STATE_IN_ENABLE |
Set this option at mcuxClCss_CipherOption_t.cphsie to import an external CSS state from pIV. More... | |
| #define | MCUXCLCSS_CIPHER_STATE_IN_DISABLE |
| Set this option at mcuxClCss_CipherOption_t.cphsie to not import an external CSS state. More... | |
| #define | MCUXCLCSS_CIPHER_EXTERNAL_KEY |
Set this option at mcuxClCss_CipherOption_t.extkey to use a key located in CPU memory provided by pKey. More... | |
| #define | MCUXCLCSS_CIPHER_INTERNAL_KEY |
Set this option at mcuxClCss_CipherOption_t.extkey to use a key located in CSS keystore privded by keyIdx. More... | |
| #define | MCUXCLCSS_CIPHERPARAM_ALGORITHM_AES_ECB |
| Set this option at mcuxClCss_CipherOption_t.cphmde to use AES engine in Electornic Code Book (ECB) mode. More... | |
| #define | MCUXCLCSS_CIPHERPARAM_ALGORITHM_AES_CBC |
| Set this option at mcuxClCss_CipherOption_t.cphmde to use AES engine in Cipher Block Chaining (CBC) mode. More... | |
| #define | MCUXCLCSS_CIPHERPARAM_ALGORITHM_AES_CTR |
| Set this option at mcuxClCss_CipherOption_t.cphmde to use AES engine in Counter (CTR) mode. More... | |
| #define | MCUXCLCSS_CIPHER_BLOCK_SIZE_AES |
| #define | MCUXCLCSS_CIPHER_KEY_SIZE_AES_128 |
| Size of an AES128 key: 128 bit (16 bytes) More... | |
| #define | MCUXCLCSS_CIPHER_KEY_SIZE_AES_192 |
| Size of an AES192 key: 192 bit (24 bytes) More... | |
| #define | MCUXCLCSS_CIPHER_KEY_SIZE_AES_256 |
| Size of an AES192 key: 256 bit (32 bytes) More... | |
Functions | |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t | mcuxClCss_Cipher_Async (mcuxClCss_CipherOption_t options, mcuxClCss_KeyIndex_t keyIdx, uint8_t const *pKey, size_t keyLength, uint8_t const *pInput, size_t inputLength, uint8_t *pIV, uint8_t *pOutput) |
| Performs AES encryption/decryption. More... | |
CSSv2 header for symmetric ciphers.
This header exposes functions that enable using the CSSv2 for symmetric encryption/decryption. The cipher algorithm supported by CSSv2 is AES in the following modes: