CSSv2 header for key management. More...
#include <mcuxClCss_Common.h>Go to the source code of this file.
Data Structures | |
| union | mcuxClCss_KeyImportOption_t |
| Command option bit field for mcuxClCss_KeyImport_Async. More... | |
Macros | |
| #define | MCUXCLCSS_KEYIMPORT_VALUE_KFMT_UDF |
| Key format UDF with shares in RTL or memory. More... | |
| #define | MCUXCLCSS_KEYIMPORT_VALUE_KFMT_RFC3394 |
| Key format RFC3394 with shares in memory. More... | |
| #define | MCUXCLCSS_KEYIMPORT_VALUE_KFMT_PUF |
| Key from PUF. More... | |
| #define | MCUXCLCSS_KEYIMPORT_KFMT_UDF |
| Key format UDF with shares in RTL or memory. More... | |
| #define | MCUXCLCSS_KEYIMPORT_KFMT_RFC3394 |
| Key format RFC3394 with shares in memory. More... | |
| #define | MCUXCLCSS_KEYIMPORT_KFMT_PUF |
| Key from PUF. More... | |
| #define | MCUXCLCSS_RFC3394_OVERHEAD |
| Overhead between RFC3394 blob and key size. More... | |
| #define | MCUXCLCSS_RFC3394_CONTAINER_SIZE_128 |
| Size of RFC3394 container for 128 bit key. More... | |
| #define | MCUXCLCSS_RFC3394_CONTAINER_SIZE_256 |
| Size of RFC3394 container for 256 bit key. More... | |
Functions | |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t | mcuxClCss_KeyDelete_Async (mcuxClCss_KeyIndex_t keyIdx) |
| Deletes a key from keystore at the given index. More... | |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t | mcuxClCss_KeyImport_Async (mcuxClCss_KeyImportOption_t options, uint8_t const *pImportKey, size_t importKeyLength, mcuxClCss_KeyIndex_t wrappingKeyIdx, mcuxClCss_KeyIndex_t targetKeyIdx) |
| Imports a key from external storage to an internal key register. More... | |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t | mcuxClCss_KeyExport_Async (mcuxClCss_KeyIndex_t wrappingKeyIdx, mcuxClCss_KeyIndex_t exportKeyIdx, uint8_t *pOutput) |
| Exports a key from an internal key register to external storage, using a wrapping key. More... | |
| MCUXCLCSS_API mcuxClCss_Status_Protected_t | mcuxClCss_GetKeyProperties (mcuxClCss_KeyIndex_t keyIdx, mcuxClCss_KeyProp_t *pKeyProp) |
| Exports the properties of the keys stored in the CSS internal keystore. More... | |
CSSv2 header for key management.
This header exposes functions that can be used to manage the keystore of CSSv2. This includes: