CSSv2 type header. More...
#include <stdint.h>#include <stddef.h>Go to the source code of this file.
Data Structures | |
| union | mcuxClCss_KeyProp_t |
| Type for CSS key store key properties. More... | |
Macros | |
| #define | MCUXCLCSS_KEY_SLOTS |
| Number of key slots in the CSS key store. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_KEY_SIZE_128 |
| 128-bit key More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_KEY_SIZE_256 |
| 256-bit key More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_ACTIVE |
| Key is active (loaded) More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_BASE_SLOT |
| First part of multi-slot key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_GENERAL_PURPOSE_SLOT |
| General purpose key slot. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_RETENTION_SLOT |
| Retention key slot. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_HW_OUT_SLOT |
| Hardware output key slot. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_CMAC |
| CMAC key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_KSK |
| Key signing key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_RTF |
| RTF signing key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_CKDF |
| CKDF signing key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_HKDF |
| HKDF signing key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_ECSGN |
| ECC signing key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_ECDH |
| ECC Diffie Hellman private key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_AES |
| AES key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_HMAC |
| HMAC key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_KWK |
| Key Wrapping Key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_KUOK |
| Key Unwrapping Only Key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_TLS_PREMASTER_SECRET |
| TLS Premaster Secret. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_TLS_MASTER_SECRET |
| TLS Master Secret. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_KGSRC |
| Can provide key material input for ECC key generation. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_HW_OUT |
| A key to be used in a hardware out key slot. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_WRPOK |
| The key can be wrapped. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_DUK |
| Device Unique Key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_PRIVILEGED |
| Caller must be in privileged mode to use the key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_NOTPRIVILEGED |
| Caller does not have to be in privileged mode to use the key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_SECURE |
| Caller must be in secure mode to use the key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_VALUE_NOTSECURE |
| Caller does not have to be in secure mode to use the key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_KEY_SIZE_128 |
| This value of mcuxClCss_KeyProp_t.ksize indicates a 128 bit key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_KEY_SIZE_256 |
| This value of mcuxClCss_KeyProp_t.ksize indicates a 256 bit key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_ACTIVE_TRUE |
| This value of mcuxClCss_KeyProp_t.kactv indicates that the slot contains an active key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_ACTIVE_FALSE |
| This value of mcuxClCss_KeyProp_t.kactv indicates that the slot does not contain active key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_BASE_SLOT |
| This value of mcuxClCss_KeyProp_t.kbase indicates that the slot is the base slot of a 2-slot key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_SECOND_SLOT |
| This value of mcuxClCss_KeyProp_t.kbase indicates that the slot is the second slot of a 2-slot key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_GENERAL_PURPOSE_SLOT_TRUE |
| This value of mcuxClCss_KeyProp_t.fgp indicates that the slot is a retention key slot or a hardware out key slot. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_GENERAL_PURPOSE_SLOT_FALSE |
| This value of mcuxClCss_KeyProp_t.fgp indicates that the slot is a neither retention key slot nor hardware out key slot. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_RETENTION_SLOT_TRUE |
| This value of mcuxClCss_KeyProp_t.frtn indicates that the slot is a retention key slot. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_RETENTION_SLOT_FALSE |
| This value of mcuxClCss_KeyProp_t.frtn indicates that the slot is not a retention key slot. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_HW_OUT_SLOT_TRUE |
| This value of mcuxClCss_KeyProp_t.fhwo indicates that the slot is a hardware out key slot. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_HW_OUT_SLOT_FALSE |
| This value of mcuxClCss_KeyProp_t.fhwo indicates that the slot is not a hardware out key slot. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_CMAC_TRUE |
| This value of mcuxClCss_KeyProp_t.ucmac indicates that the key can be used for CMAC. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_CMAC_FALSE |
| This value of mcuxClCss_KeyProp_t.ucmac indicates that the key cannot be used for CMAC. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_KSK_TRUE |
| This value of mcuxClCss_KeyProp_t.uksk indicates that the key can be used for key signing. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_KSK_FALSE |
| This value of mcuxClCss_KeyProp_t.uksk indicates that the key cannot be used for key signing. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_RTF_TRUE |
| This value of mcuxClCss_KeyProp_t.urtf indicates that the key can be used for RTF signing. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_RTF_FALSE |
| This value of mcuxClCss_KeyProp_t.urtf indicates that the key cannot be used for RTF signing. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_CKDF_TRUE |
| This value of mcuxClCss_KeyProp_t.uckdf indicates that the key can be used for CKDF. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_CKDF_FALSE |
| This value of mcuxClCss_KeyProp_t.uckdf indicates that the key cannot be used for CKDF. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_HKDF_TRUE |
| This value of mcuxClCss_KeyProp_t.uhkdf indicates that the key can be used for HKDF. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_HKDF_FALSE |
| This value of mcuxClCss_KeyProp_t.uhkdf indicates that the key cannot be used for HKDF. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_ECC_TRUE |
| This value of mcuxClCss_KeyProp_t.uecsg indicates that the key can be used for ECC signing. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_ECC_FALSE |
| This value of mcuxClCss_KeyProp_t.uecsg indicates that the key cannot be used for ECC signing. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_ECC_DH_PRIVATE_TRUE |
| This value of mcuxClCss_KeyProp_t.uecdh indicates that the key is a ECC Diffie Hellman private key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_ECC_DH_PRIVATE_FALSE |
| This value of mcuxClCss_KeyProp_t.uecdh indicates that the key is not an ECC Diffie Hellman private key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_AES_TRUE |
| This value of mcuxClCss_KeyProp_t.uaes indicates that the key is an AES key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_AES_FALSE |
| This value of mcuxClCss_KeyProp_t.uaes indicates that the key is not an AES key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_HMAC_TRUE |
| This value of mcuxClCss_KeyProp_t.uhmac indicates that the key is an HMAC key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_HMAC_FALSE |
| This value of mcuxClCss_KeyProp_t.uhmac indicates that the key is not an HMAC key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_KWK_TRUE |
| This value of mcuxClCss_KeyProp_t.ukwk indicates that the key is a Key Wrapping Key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_KWK_FALSE |
| This value of mcuxClCss_KeyProp_t.ukwk indicates that the key is not a Key Wrapping Key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_KUOK_TRUE |
| This value of mcuxClCss_KeyProp_t.ukuok indicates that the key is a Key Unwrapping Only Key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_KUOK_FALSE |
| This value of mcuxClCss_KeyProp_t.ukuok indicates that the key is not a Key Unwrapping Only Key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_TLS_PREMASTER_SECRET_TRUE |
| This value of mcuxClCss_KeyProp_t.utlspms indicates that the key is a TLS Premaster Secret. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_TLS_PREMASTER_SECRET_FALSE |
| This value of mcuxClCss_KeyProp_t.utlspms indicates that the key is not a TLS Premaster Secret. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_TLS_MASTER_SECRET_TRUE |
| This value of mcuxClCss_KeyProp_t.utlsms indicates that the key is a TLS Master Secret. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_TLS_MASTER_SECRET_FALSE |
| This value of mcuxClCss_KeyProp_t.utlsms indicates that the key is not a TLS Master Secret. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_INPUT_FOR_ECC_TRUE |
| This value of mcuxClCss_KeyProp_t.ukgsrc indicates that the key can be used as key material input for ECC key generation. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_INPUT_FOR_ECC_FALSE |
| This value of mcuxClCss_KeyProp_t.ukgsrc indicates that the key cannot be used as key material input for ECC key generation. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_HW_OUT_TRUE |
| This value of mcuxClCss_KeyProp_t.uhwo indicates that the key can be used in a hardware out key slot. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_HW_OUT_FALSE |
| This value of mcuxClCss_KeyProp_t.uhwo indicates that the key cannot be used in a hardware out key slot. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_WRAP_TRUE |
| This value of mcuxClCss_KeyProp_t.wrpok indicates that the key can be wrapped. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_WRAP_FALSE |
| This value of mcuxClCss_KeyProp_t.wrpok indicates that the key cannot be wrapped. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_DEVICE_UNIQUE_TRUE |
| This value of mcuxClCss_KeyProp_t.duk indicates that the key is a Device Unique Key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_DEVICE_UNIQUE_FALSE |
| This value of mcuxClCss_KeyProp_t.duk indicates that the key is not a Device Unique Key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_PRIVILEGED_TRUE |
| This value of mcuxClCss_KeyProp_t.upprot_priv indicates that the caller must be in privileged mode to use the key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_PRIVILEGED_FALSE |
| This value of mcuxClCss_KeyProp_t.upprot_priv indicates that the caller does not need to be in privileged mode to use the key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_SECURE_TRUE |
| This value of mcuxClCss_KeyProp_t.upprot_sec indicates that the caller must be in secure mode to use the key. More... | |
| #define | MCUXCLCSS_KEYPROPERTY_SECURE_FALSE |
| This value of mcuxClCss_KeyProp_t.upprot_sec indicates that the caller does not need to be in secure mode to use the key. More... | |
| #define | MCUXCLCSS_STATUS_OK |
| No error occurred. More... | |
| #define | MCUXCLCSS_STATUS_OK_WAIT |
An _Async function successfully started a CSS command. Call mcuxClCss_WaitForOperation to complete it. More... | |
| #define | MCUXCLCSS_STATUS_HW_FAULT |
| CSSv2 hardware detected a fault. More... | |
| #define | MCUXCLCSS_STATUS_HW_ALGORITHM |
| An algorithm failed in hardware. More... | |
| #define | MCUXCLCSS_STATUS_HW_OPERATIONAL |
| CSSv2 was operated incorrectly. More... | |
| #define | MCUXCLCSS_STATUS_HW_BUS |
| A bus access failed. More... | |
| #define | MCUXCLCSS_STATUS_HW_INTEGRITY |
| An integrity check failed in hardware. More... | |
| #define | MCUXCLCSS_STATUS_HW_PRNG |
| Read access to PRNG output while PRNG is not in ready state. More... | |
| #define | MCUXCLCSS_STATUS_HW_DTRNG |
| Unable to get entropy from dTRNG with current configuration. More... | |
| #define | MCUXCLCSS_STATUS_SW_FAULT |
| Software detected a fault. More... | |
| #define | MCUXCLCSS_STATUS_SW_CANNOT_INTERRUPT |
| A CSS command was started while the CSS was still busy, or a SHA-Direct command was started while the SHA kernel was still busy. More... | |
| #define | MCUXCLCSS_STATUS_SW_INVALID_PARAM |
| Incorrect parameters were supplied. More... | |
| #define | MCUXCLCSS_STATUS_SW_INVALID_STATE |
| This can happen when CSS is in a wrong state for the requested CSS command. More... | |
| #define | MCUXCLCSS_STATUS_SW_COUNTER_EXPIRED |
| A software counter expired while waiting for a CSS operation to finish. More... | |
| #define | MCUXCLCSS_STATUS_SW_COMPARISON_FAILED |
| A comparison between a CSS flag and its expected value failed. More... | |
| #define | MCUXCLCSS_STATUS_IS_HW_ERROR(x) |
| Checks whether an error code is a hardware error. Indicates that an error was reported by CSSv2 hardware. More... | |
| #define | MCUXCLCSS_STATUS_IS_SW_ERROR(x) |
| Checks whether an error code is a software error. Indicates that the error was detected by the driver software and not by CSSv2 hardware. More... | |
| #define | utlpsms |
| Deprecated name for mcuxClCss_KeyProp_t.utlspms. More... | |
Typedefs | |
| typedef uint64_t | mcuxClCss_Status_Protected_t |
| Type for CSS driver protected status codes. More... | |
| typedef uint32_t | mcuxClCss_Status_t |
| Type for CSS driver status codes. More... | |
| typedef uint8_t | mcuxClCss_KeyIndex_t |
| Type for CSS keystore indices. More... | |
| typedef mcuxClCss_Status_t(* | mcuxClCss_TransferToRegisterFunction_t) (uint32_t volatile *destRegister, uint8_t const *source, size_t size, void *pCallerData) |
| Function type for transfer of data to a memory-mapped register. More... | |
CSSv2 type header.
This header defines types that are used by other mcuxClCss headers.