Defines the memory consumption for the mcuxClEcc component. More...
Go to the source code of this file.
Macros | |
| #define | MCUXCLECC_KEYGEN_WACPU_SIZE |
| CPU workarea size (in bytes) for mcuxClEcc_KeyGen. More... | |
| #define | MCUXCLECC_SIGN_WACPU_SIZE |
| CPU workarea size (in bytes) for mcuxClEcc_Sign. More... | |
| #define | MCUXCLECC_VERIFY_WACPU_SIZE |
| CPU workarea size (in bytes) for mcuxClEcc_Verify. More... | |
| #define | MCUXCLECC_POINTMULT_WACPU_SIZE |
| CPU workarea size (in bytes) for mcuxClEcc_PointMult. More... | |
| #define | MCUXCLECC_PKC_WORDSIZE |
| PKC wordsize in ECC component. More... | |
| #define | MCUXCLECC_MAX(value0, value1) |
| Helper macro to get the maximum of two given constants. More... | |
| #define | MCUXCLECC_ALIGN_SIZE_PKC(size) |
| Helper macro to calculate size aligned to PKC word. More... | |
| #define | MCUXCLECC_KEYGEN_WAPKC_SIZE(pByteLen, nByteLen) |
| PKC workarea size (in bytes) for mcuxClEcc_KeyGen for arbitrary lengths of p and n (in bytes). More... | |
| #define | MCUXCLECC_SIGN_WAPKC_SIZE(pByteLen, nByteLen) |
| PKC workarea size (in bytes) for mcuxClEcc_Sign for arbitrary lengths of p and n (in bytes). More... | |
| #define | MCUXCLECC_VERIFY_WAPKC_SIZE(pByteLen, nByteLen) |
| PKC workarea size (in bytes) for mcuxClEcc_Verify for arbitrary lengths of p and n (in bytes). More... | |
| #define | MCUXCLECC_POINTMULT_WAPKC_SIZE(pByteLen, nByteLen) |
| PKC workarea size (in bytes) for mcuxClEcc_PointMult for arbitrary lengths of p and n (in bytes). More... | |
Defines the memory consumption for the mcuxClEcc component.