Top-level API of the mcuxClHash component. More...
Go to the source code of this file.
Functions | |
| mcuxClHash_Status_Protected_t | mcuxClHash_compute (mcuxClSession_Handle_t session, const mcuxClHash_Algo_t *algo, const uint8_t *const in, uint32_t inSize, uint8_t *const hash, uint8_t *const rtf) |
| One-shot hash computation. More... | |
| mcuxClHash_Status_Protected_t | mcuxClHash_init (mcuxClSession_Handle_t session, mcuxClHash_Context_t *context, const mcuxClHash_Algo_t *algo) |
| Initializes the context for a new hash computation. More... | |
| mcuxClHash_Status_Protected_t | mcuxClHash_update (mcuxClSession_Handle_t session, mcuxClHash_Context_t *context, const uint8_t *const in, uint32_t inSize) |
| Adds a chunk of data to an ongoing hash computation. More... | |
| mcuxClHash_Status_Protected_t | mcuxClHash_finish (mcuxClSession_Handle_t session, mcuxClHash_Context_t *context, uint8_t *const hash, uint8_t *const rtf) |
| Finishes a hash computation. More... | |
Top-level API of the mcuxClHash component.