Example for the mcuxClKey component. More...
#include <mcuxClKey.h>#include <mcuxClSession.h>#include <mcuxCsslFlowProtection.h>#include <stdbool.h>Functions | |
| bool | mcuxClKey_example (void) |
| Performs an example initialization and cleanup of the mcuxClKey component. More... | |
Variables | |
| static uint8_t | aes128_key [MCUXCLKEY_SIZE_128] |
Example for the mcuxClKey component.
| bool mcuxClKey_example | ( | void | ) |
Performs an example initialization and cleanup of the mcuxClKey component.
| true | The example code completed successfully |
| false | The example code failed |