Top-level API of the mcuxClMac component. More...
Go to the source code of this file.
Functions | |
| mcuxClMac_Status_Protected_t | mcuxClMac_compute (mcuxClSession_Handle_t session, const mcuxClKey_Handle_t key, const mcuxClMac_Mode_t mode, const uint8_t *const in, uint32_t inSize, uint8_t *const mac) |
| One-shot message authentication code (MAC) computation. More... | |
| mcuxClMac_Status_Protected_t | mcuxClMac_init (mcuxClSession_Handle_t session, mcuxClMac_Context_t *const context, const mcuxClKey_Handle_t key, const mcuxClMac_Mode_t mode) |
| Initialization for a multipart MAC computation. More... | |
| mcuxClMac_Status_Protected_t | mcuxClMac_process (mcuxClSession_Handle_t session, mcuxClMac_Context_t *const context, const uint8_t *const in, uint32_t inSize) |
| Data processing for a multipart MAC computation. More... | |
| mcuxClMac_Status_Protected_t | mcuxClMac_finish (mcuxClSession_Handle_t session, mcuxClMac_Context_t *const context, uint8_t *const mac) |
| MAC generation for a multipart MAC computation. More... | |
Top-level API of the mcuxClMac component.