APIs of mcuxClMath component. More...
#include <stdint.h>#include <stdbool.h>#include <mcuxCsslFlowProtection.h>#include <mcuxClPkc.h>#include <mcuxClMath_Types.h>Go to the source code of this file.
Macros | |
| #define | MCUXCLMATH_FP_INITLOCALUPTRT(i3_i2_i1_i0, i7_i6_i5_i4, localPtrUptrt, noOfIndices) |
| Helper macro to call mcuxClMath_InitLocalUptrt with flow protection. More... | |
| #define | MCUXCLMATH_FP_LEADINGZEROS(iX) |
| Helper macro to call mcuxClMath_LeadingZeros with flow protection. More... | |
| #define | MCUXCLMATH_FP_TRAILINGZEROS(iX) |
| Helper macro to call mcuxClMath_TrailingZeros with flow protection. More... | |
| #define | MCUXCLMATH_SHIFTMODULUS(iNShifted, iN) |
| Helper macro for mcuxClMath_ShiftModulus. More... | |
| #define | MCUXCLMATH_FP_SHIFTMODULUS(iNShifted, iN) |
| Helper macro for mcuxClMath_ShiftModulus with flow protection. More... | |
| #define | MCUXCLMATH_NDASH(iN, iT) |
| Helper macro for mcuxClMath_NDash. More... | |
| #define | MCUXCLMATH_FP_NDASH(iN, iT) |
| Helper macro for mcuxClMath_NDash with flow protection. More... | |
| #define | MCUXCLMATH_QDASH(iQDash, iNShifted, iN, iT, len) |
| Helper macro for mcuxClMath_QDash. More... | |
| #define | MCUXCLMATH_FP_QDASH(iQDash, iNShifted, iN, iT, len) |
| Helper macro for mcuxClMath_QDash with flow protection. More... | |
| #define | MCUXCLMATH_QSQUARED(iQSqr, iNShifted, iN, iT) |
| Helper macro for mcuxClMath_QSquared. More... | |
| #define | MCUXCLMATH_FP_QSQUARED(iQSqr, iNShifted, iN, iT) |
| Helper macro for mcuxClMath_QSquared with flow protection. More... | |
| #define | MCUXCLMATH_MODINV(iR, iX, iN, iT) |
| Helper macro for mcuxClMath_ModInv. More... | |
| #define | MCUXCLMATH_FP_MODINV(iR, iX, iN, iT) |
| Helper macro for mcuxClMath_ModInv with flow protection. More... | |
| #define | MCUXCLMATH_REDUCEMODEVEN(iR, iX, iN, iT0, iT1, iT2, iT3) |
| Helper macro for mcuxClMath_ReduceModEven. More... | |
| #define | MCUXCLMATH_FP_REDUCEMODEVEN(iR, iX, iN, iT0, iT1, iT2, iT3) |
| Helper macro for mcuxClMath_ReduceModEven with flow protection. More... | |
| #define | MCUXCLMATH_MODEXP_SQRMULTL2R(pExp, byteLenExp, iR, iX, iN, iT) |
| Helper macro for mcuxClMath_ModExp_SqrMultL2R. More... | |
| #define | MCUXCLMATH_FP_MODEXP_SQRMULTL2R(pExp, byteLenExp, iR, iX, iN, iT) |
| Helper macro for mcuxClMath_ModExp_SqrMultL2R with flow protection. More... | |
| #define | MCUXCLMATH_SECMODEXP(pExp, pExpTemp, byteLenExp, iR, iX, iN, iTE, iT0, iT1, iT2, iT3) |
| Helper macro for mcuxClMath_SecModExp. More... | |
| #define | MCUXCLMATH_FP_SECMODEXP(pExp, pExpTemp, byteLenExp, iR, iX, iN, iTE, iT0, iT1, iT2, iT3) |
| Helper macro for mcuxClMath_SecModExp with flow protection. More... | |
| #define | MCUXCLMATH_EXACTDIVIDEODD(iR, iX, iN, iT, pkcByteLenX, pkcByteLenY) |
| Helper macro for mcuxClMath_ExactDivideOdd. More... | |
| #define | MCUXCLMATH_FP_EXACTDIVIDEODD(iR, iX, iN, iT, pkcByteLenX, pkcByteLenY) |
| Helper macro for mcuxClMath_ExactDivideOdd with flow protection. More... | |
| #define | MCUXCLMATH_EXACTDIVIDE(iR, iX, iN, iT, pkcByteLenX, pkcByteLenY) |
| Helper macro for mcuxClMath_ExactDivide. More... | |
| #define | MCUXCLMATH_FP_EXACTDIVIDE(iR, iX, iN, iT, pkcByteLenX, pkcByteLenY) |
| Helper macro for mcuxClMath_ExactDivide with flow protection. More... | |
Functions | |
| mcuxClMath_Status_Protected_t | mcuxClMath_InitLocalUptrt (uint32_t i3_i2_i1_i0, uint32_t i7_i6_i5_i4, uint16_t *localPtrUptrt, uint8_t noOfIndices, const uint16_t **oldPtrUptrt) |
| Initializes the new UPTRT and returns the address of existing UPTRT. More... | |
| mcuxClMath_Status_Protected_t | mcuxClMath_LeadingZeros (uint8_t iX, uint32_t *nLeadingZeros) |
| Counts number of leading zeros of operand in the given buffer (length = ps1 OPLEN). More... | |
| mcuxClMath_Status_Protected_t | mcuxClMath_TrailingZeros (uint8_t iX, uint32_t *nTrailingZeros) |
| Counts number of trailing zeros of operand in the given buffer (length = ps1 OPLEN). More... | |
| mcuxClMath_Status_Protected_t | mcuxClMath_ShiftModulus (uint16_t iNShifted_iN) |
| Left shifts modulus until most significant bit of the buffer (length = ps1 OPLEN) is 1, and stores the result in the buffer specified. More... | |
| mcuxClMath_Status_Protected_t | mcuxClMath_NDash (uint16_t iN_iT) |
| Prepares modulus buffer (initializes NDash) to be used in modular multiplication (inversion, ...) with odd modulus. More... | |
| mcuxClMath_Status_Protected_t | mcuxClMath_QDash (uint32_t iQDash_iNShifted_iN_iT, uint16_t len) |
| Calculates Q * Q' mod n, where Q = 256^(ps1 OPLEN) mod n, and Q' = 256^len mod n. More... | |
| mcuxClMath_Status_Protected_t | mcuxClMath_QSquared (uint32_t iQSqr_iNShifted_iN_iT) |
| Calculates Q^2 mod n, where Q = 256^(ps1 OPLEN) mod n. More... | |
| mcuxClMath_Status_Protected_t | mcuxClMath_ModInv (uint32_t iR_iX_iN_iT) |
| Calculates modular inversion, X^(-1) mod n. More... | |
| mcuxClMath_Status_Protected_t | mcuxClMath_ReduceModEven (uint32_t iR_iX_iN_iT0, uint32_t iT1_iT2_iT3) |
| Calculates modular reduction with even modulus, x mod n, where n is even. More... | |
| mcuxClMath_Status_Protected_t | mcuxClMath_ModExp_SqrMultL2R (const uint8_t *pExp, uint32_t byteLenExp, uint32_t iR_iX_iN_iT) |
| Calculates modular exponentiation with left-to-right binary square and multiply algorithm. More... | |
| mcuxClMath_Status_Protected_t | mcuxClMath_SecModExp (const uint8_t *pExp, uint32_t *pExpTemp, uint32_t byteLenExp, uint32_t iT3_iX_iT2_iT1, uint32_t iN_iTE_iT0_iR) |
| Securely calculates modular exponentiation. More... | |
| mcuxClMath_Status_Protected_t | mcuxClMath_ExactDivideOdd (uint32_t iR_iX_iY_iT, uint32_t pkcByteLenX, uint32_t pkcByteLenY) |
| TODO 1.pkcByteLenX and pkcByteLenY shall be a multiple of pkc wordsize. More... | |
| mcuxClMath_Status_Protected_t | mcuxClMath_ExactDivide (uint32_t iR_iX_iY_iT, uint32_t pkcByteLenX, uint32_t pkcByteLenY) |
| Exact division. More... | |
APIs of mcuxClMath component.