Memory header for set function. More...
Go to the source code of this file.
Functions | |
| mcuxClMemory_Status_Protected_t | mcuxClMemory_set (uint8_t *dst, uint8_t val, size_t len, size_t buflen) |
| Sets all bytes of a memory buffer to a specified value. More... | |
Memory header for set function.
This header exposes functions that enable using memory set functions.