Top-level API of the mcuxClRsa component. More...
#include <mcuxClSession.h>#include <mcuxCsslFlowProtection.h>#include <mcuxClHash.h>#include <mcuxClRsa_Types.h>Go to the source code of this file.
Functions | |
| mcuxClRsa_Status_Protected_t | mcuxClRsa_sign (mcuxClSession_Handle_t pSession, const mcuxClRsa_Key *const pKey, const uint8_t *const pMessageOrDigest, const uint32_t messageLength, const mcuxClRsa_SignVerifyMode pPaddingMode, const uint32_t saltLength, const uint32_t options, uint8_t *const pSignature) |
| RSA sign operation. More... | |
| mcuxClRsa_Status_Protected_t | mcuxClRsa_verify (mcuxClSession_Handle_t pSession, const mcuxClRsa_Key *const pKey, const uint8_t *const pMessageOrDigest, const uint32_t messageLength, uint8_t *const pSignature, const mcuxClRsa_SignVerifyMode pVerifyMode, const uint32_t saltLength, const uint32_t options, uint8_t *const pOutput) |
| RSA verify operation. More... | |
Top-level API of the mcuxClRsa component.