Top-level API of the mcuxClSession component. More...
Go to the source code of this file.
Functions | |
| mcuxClSession_Status_Protected_t | mcuxClSession_init (mcuxClSession_Handle_t session, uint32_t *const cpuWaBuffer, uint32_t cpuWaSize, uint32_t *const pkcWaBuffer, uint32_t pkcWaSize) |
| Initialize a Crypto Library session. More... | |
| mcuxClSession_Status_Protected_t | mcuxClSession_setRtf (mcuxClSession_Handle_t session, mcuxClSession_Rtf_t RtfOptions) |
| Set the RTF option in a Crypto Library session. More... | |
| mcuxClSession_Status_Protected_t | mcuxClSession_cleanup (mcuxClSession_Handle_t session) |
| Clean up a Crypto Library session. More... | |
| mcuxClSession_Status_Protected_t | mcuxClSession_destroy (mcuxClSession_Handle_t session) |
| Destroy a Crypto Library session. More... | |
Top-level API of the mcuxClSession component.