Include file for constant time memory compare function. More...
#include <stdint.h>#include <stdlib.h>#include <mcuxCsslParamIntegrity.h>#include <mcuxCsslFlowProtection.h>Go to the source code of this file.
Macros | |
| #define | MCUXCSSLMEMORY_COMPARE_EQUAL |
| The two contents are equal. More... | |
| #define | MCUXCSSLMEMORY_COMPARE_NOT_EQUAL |
| The two contents are not equal. More... | |
| #define | MCUXCSSLMEMORY_COMPARE_INVALID_PARAMETER |
| A parameter was invalid. More... | |
| #define | MCUXCSSLMEMORY_COMPARE_FAULT |
| A fault occurred in the execution of mcuxCsslMemory_Compare. More... | |
Typedefs | |
| typedef uint64_t | mcuxCsslMemory_CompareResult_t |
| return type for CSSL Memory compare More... | |
Functions | |
| mcuxCsslMemory_CompareResult_t | mcuxCsslMemory_Compare (mcuxCsslParamIntegrity_Checksum_t chk, void const *lhs, void const *rhs, size_t cnt) |
Compares the two memory regions lhs and rhs. More... | |
Include file for constant time memory compare function.