![]() |
Maestro Audio Framework
v 1.0
NXP Semiconductors
|
| af_error.h | Contains error and logging definitions for Af |
| container.h | Contains macros and functions that are common and generic across OSA container data types |
| error.h | Contains common error codes and definitions |
| file_utils.h | This file provides file manipulation functions |
| general_utils.h | This file provides general helper functions |
| logging.h | Contains logging prototypes and definitions for the connected radio |
| memtypes.h | Contains mem types definitions for all modules in impresario |
| metadata_error.h | Contains error and logging definitions for Metadata |
| osa_common.h | Primary include for libosa |
| osa_cond.h | Contains condition variable (CV) function prototypes |
| osa_dir.h | Contains file and directory function prototypes for libosa |
| osa_event.h | Contains timeout/event function prototypes for Impresario libosa |
| osa_freertos.h | Header includes specific to FreeRTOS |
| osa_init.h | Contains initialization function prototypes for libosa |
| osa_isr.h | Contains OSA functions related to ISR management |
| osa_memory.h | Contains memory allocation function prototypes for Maestro libosa |
| osa_message.h | Contains message queue function prototypes for libosa |
| osa_misc.h | Contains miscellaneous function prototypes for libosa |
| osa_mutex.h | Contains mutex function prototypes for Impresario libosa |
| osa_sem.h | Contains semaphore function prototypes for Impresario libosa |
| osa_thread.h | Contains thread function prototypes for libosa |
| osa_time.h | Contains time function prototypes for libosa |
| osa_types.h | Contains base data types for NXP libosa |
| ringbuffer.h | Implements a data ringbuffer |
| streamer_api.h | Streamer API header |
| streamer_element_properties.h | Header for streamer element properties |
| streamer_error.h | Contains error and logging definitions for streamer |
| streamer_message.h | This file includes definitions for messages used by the Streamer library |
| streamer_pcm.h | Streamer PCM API header |
| vector.h | Vector data type implementation |