This file provides general helper functions.
More...
#include <stdint.h>
|
| int32_t | smallest_int (int32_t a, int32_t b) |
| | smallest_int More...
|
| |
| uint32_t | _transform_16_to_32 (void *src, uint32_t src_len, void *dst, uint32_t dst_len) |
| | Extend 16 bit per sample to 32bit per sample. More...
|
| |
| uint32_t | _transform_24_to_32 (void *src, uint32_t src_len, void *dst, uint32_t dst_len) |
| | Extend 24 bit per sample to 32bit per sample. More...
|
| |
| uint32_t | _transform_32_to_24 (void *src, uint32_t src_len, void *dst, uint32_t dst_len) |
| | Compress 32 bit per sample to 24 bit per sample. More...
|
| |
| uint32_t | _transform_32_to_16 (void *src, uint32_t src_len, void *dst, uint32_t dst_len) |
| | Compress 32 bit per sample to 16 bit per sample. More...
|
| |
| uint32_t | data_copy_32bits (void *src, uint32_t src_len, void *dst, uint32_t dst_len) |
| | Equivalent to a memcpy used with src and dest size validation to determine the amount of bytes to copy. More...
|
| |
| uint32_t | _interleave_16_to_32 (void *src, uint32_t src_len, void *dst, uint32_t dst_len) |
| | Used to interleave samples from two input buffers on an output buffer. More...
|
| |
| uint32_t | _interleave_24_to_32 (void *src, uint32_t src_len, void *dst, uint32_t dst_len) |
| | Used to interleave samples from two input buffers on an output buffer. More...
|
| |
| uint32_t | _interleave_32bits (void *src, uint32_t src_len, void *dst, uint32_t dst_len) |
| | Used to interleave samples from two input buffers on an output buffer. More...
|
| |
◆ smallest_int()
| int32_t smallest_int |
( |
int32_t |
a, |
|
|
int32_t |
b |
|
) |
| |
Function to determine the smallest of two integers.
- Parameters
-
| a | first integer |
| b | second integer |
- Returns
- value of the smallest integer
◆ _transform_16_to_32()
| uint32_t _transform_16_to_32 |
( |
void * |
src, |
|
|
uint32_t |
src_len, |
|
|
void * |
dst, |
|
|
uint32_t |
dst_len |
|
) |
| |
- Parameters
-
| src | [IN] 16bit sample's buffer |
| src_len | [IN] Number of bytes in the input |
| dst | [OUT] Output buffer where the 32-bit data is going to be written |
| dst_len | [IN] Maximum num of bytes that should be written on the output |
- Returns
- uint32_t Number of bytes that were written in the destination buffer
This function uses src_len as the number byes and the number of bytes in dst_len to determine how many bytes will be copied in the output buffer dst. The return value will be the number in bytes that was copied to the out buffer
◆ _transform_24_to_32()
| uint32_t _transform_24_to_32 |
( |
void * |
src, |
|
|
uint32_t |
src_len, |
|
|
void * |
dst, |
|
|
uint32_t |
dst_len |
|
) |
| |
- Parameters
-
| src | [IN] 24 bit sample's buffer |
| src_len | [IN] Number of bytes in the input |
| dst | [OUT] Output buffer where the 32-bit data is going to be written |
| dst_len | [IN] Maximum num of bytes that should be written on the output |
- Returns
- uint32_t Number of bytes that were written in the destination buffer
This function uses src_len as the number byes and the number of bytes in dst_len to determine how many bytes will be copied in the output buffer dst. The return value will be the number in bytes that was copied to the out buffer
◆ _transform_32_to_24()
| uint32_t _transform_32_to_24 |
( |
void * |
src, |
|
|
uint32_t |
src_len, |
|
|
void * |
dst, |
|
|
uint32_t |
dst_len |
|
) |
| |
- Parameters
-
| src | [IN] 32 bit sample's buffer |
| src_len | [IN] Number of bytes in the input |
| dst | [OUT] Output buffer where the 24-bit data is going to be written |
| dst_len | [IN] Maximum num of bytes that should be written on the output |
- Returns
- uint32_t Number of bytes that were written in the destination buffer
This function uses src_len as the number byes and the number of bytes in dst_len to determine how many bytes will be copied in the output buffer dst. The return value will be the number in bytes that was copied to the out buffer
◆ _transform_32_to_16()
| uint32_t _transform_32_to_16 |
( |
void * |
src, |
|
|
uint32_t |
src_len, |
|
|
void * |
dst, |
|
|
uint32_t |
dst_len |
|
) |
| |
- Parameters
-
| src | [IN] 32 bit sample's buffer |
| src_len | [IN] Number of bytes in the input |
| dst | [OUT] Output buffer where the 16-bit data is going to be written |
| dst_len | [IN] Maximum num of bytes that should be written on the output |
- Returns
- uint32_t Number of bytes that were written in the destination buffer
This function uses src_len as the number byes and the number of bytes in dst_len to determine how many bytes will be copied in the output buffer dst. The return value will be the number in bytes that was copied to the out buffer
◆ data_copy_32bits()
| uint32_t data_copy_32bits |
( |
void * |
src, |
|
|
uint32_t |
src_len, |
|
|
void * |
dst, |
|
|
uint32_t |
dst_len |
|
) |
| |
- Parameters
-
| src | [IN] 32 bit sample's buffer |
| src_len | [IN] Number of bytes in the input |
| dst | [OUT] Output buffer where the 32-bit data is going to be written |
| dst_len | [IN] Maximum num of bytes that should be written on the output |
- Returns
- uint32_t Number of bytes that were written in the destination buffer
◆ _interleave_16_to_32()
| uint32_t _interleave_16_to_32 |
( |
void * |
src, |
|
|
uint32_t |
src_len, |
|
|
void * |
dst, |
|
|
uint32_t |
dst_len |
|
) |
| |
- Parameters
-
| src | [IN] 16 bit sample's buffer |
| src_len | [IN] Number of bytes in the input. |
| dst | [OUT] Output buffer where the 32-bit data is going to be written |
| dst_len | [IN] Maximum num of bytes that should be written on the output |
- Returns
- uint32_t Number of bytes that were written in the destination buffer
◆ _interleave_24_to_32()
| uint32_t _interleave_24_to_32 |
( |
void * |
src, |
|
|
uint32_t |
src_len, |
|
|
void * |
dst, |
|
|
uint32_t |
dst_len |
|
) |
| |
- Parameters
-
| src | [IN] 24 bit sample's buffer |
| src_len | [IN] Number of bytes in the input. |
| dst | [OUT] Output buffer where the 32-bit data is going to be written |
| dst_len | [IN] Maximum num of bytes that should be written on the output |
- Returns
- uint32_t Number of bytes that were written in the destination buffer
◆ _interleave_32bits()
| uint32_t _interleave_32bits |
( |
void * |
src, |
|
|
uint32_t |
src_len, |
|
|
void * |
dst, |
|
|
uint32_t |
dst_len |
|
) |
| |
- Parameters
-
| src | [IN] 32 bit sample's buffer |
| src_len | [IN] Number of bytes in the input. Applies to both input buffers |
| dst | [OUT] Output buffer where the 32-bit data is going to be written |
| dst_len | [IN] Maximum num of bytes that should be written on the output |
- Returns
- uint32_t Number of bytes that were written in the destination buffer