![]() |
Maestro Audio Framework
v 1.0
NXP Semiconductors
|
Contains thread function prototypes for libosa. More...
Data Structures | |
| struct | OsaThreadAttr |
| Thread Attributes. More... | |
Macros | |
| #define | OSA_MAX_THREAD_NAME_LENGTH 40 |
Enumerations | |
| enum | OsaSchedPriority { OSA_SCHED_PRIORITY_LOW = 0 , OSA_SCHED_PRIORITY_NORMAL , OSA_SCHED_PRIORITY_HIGH , OSA_SCHED_PRIORITY_URGENT } |
| Scheduler Priority Enumeration of possible priorities for thread scheduling. More... | |
| enum | OsaSchedPolicy { OSA_SCHED_POLICY_FIFO = 0 , OSA_SCHED_POLICY_RR , OSA_SCHED_POLICY_OTHER } |
| Scheduler Policy Enumeration of scheduling policies for threads. More... | |
Functions | |
| int | osa_thread_attr_init (OsaThreadAttr *attr) |
| Initialize a thread attribute structure. More... | |
| void | osa_thread_attr_destroy (OsaThreadAttr *attr) |
| Destroy a thread attribute structure. More... | |
| int | osa_thread_attr_set_stack_size (OsaThreadAttr *attr, size_t size) |
| Set thread attribute maximum stack size. More... | |
| int | osa_thread_attr_get_stack_size (const OsaThreadAttr *attr, size_t *size) |
| Get thread attribute maximum stack size. More... | |
| int | osa_thread_attr_set_sched_policy (OsaThreadAttr *attr, OsaSchedPolicy policy) |
| Set thread attribute scheduling policy. More... | |
| int | osa_thread_attr_get_sched_policy (const OsaThreadAttr *attr, OsaSchedPolicy *policy) |
| Get thread attribute scheduling policy. More... | |
| int | osa_thread_attr_set_sched_priority (OsaThreadAttr *attr, OsaSchedPriority priority) |
| Set thread attribute scheduling priority. More... | |
| int | osa_thread_attr_get_sched_priority (const OsaThreadAttr *attr, OsaSchedPriority *priority) |
| Get thread attribute scheduling priority. More... | |
| int | osa_thread_attr_set_sched_interval (OsaThreadAttr *attr, uint32_t interval) |
| Set thread attribute scheduling interval. More... | |
| int | osa_thread_attr_get_sched_interval (const OsaThreadAttr *attr, uint32_t *interval) |
| Get thread attribute scheduling interval. More... | |
| int | osa_thread_attr_set_name (OsaThreadAttr *attr, const char *name) |
| Set thread name attribute. More... | |
| int | osa_thread_create (OsaThread *thread, const OsaThreadAttr *attr, void(*function)(void *), void *arg) |
| Create a new thread. More... | |
| int | osa_thread_destroy (OsaThread thread) |
| Destroy a thread. More... | |
| OsaThread | osa_thread_self (void) |
| Obtain ID of the calling thread. More... | |
| int | osa_thread_join (OsaThread thread, void **value) |
| Join with a terminated thread. More... | |
| void | osa_thread_yield (void) |
| Yield a thread. More... | |
| void | osa_thread_exit (void *value) |
| Terminate a thread. More... | |
| int | osa_thread_get_id (OsaThread thread, uint32_t *tid) |
| Return an ID for a thread. More... | |
| int | osa_sched_set_policy (OsaThread thread, OsaSchedPolicy policy) |
| Set thread scheduling policy. More... | |
| int | osa_sched_get_policy (OsaThread thread, OsaSchedPolicy *policy) |
| Get thread scheduling policy. More... | |
| int | osa_sched_set_priority (OsaThread thread, OsaSchedPriority priority) |
| Set thread scheduling priority. More... | |
| int | osa_sched_get_priority (OsaThread thread, OsaSchedPriority *priority) |
| Get thread scheduling priority. More... | |
| int | osa_sched_set_rr_interval (OsaThread thread, uint32_t interval) |
| Set thread scheduling interval. More... | |
| int | osa_sched_get_rr_interval (OsaThread thread, uint32_t *interval) |
| Get thread scheduling interval. More... | |
| int | osa_thread_get_name (OsaThread thread, char **name) |
| Get thread name. More... | |
| int | osa_thread_set_name (OsaThread thread, const char *name) |
| Set thread name. More... | |
| enum OsaSchedPriority |
| enum OsaSchedPolicy |
| int osa_thread_attr_init | ( | OsaThreadAttr * | attr | ) |
Allocate memory for a thread attribute structure and initialize the parameters to default values.
| attr | Attribute structure. This will be initialized and returned as output. |
| ERRCODE_NO_ERROR | Attribute structure successfully initialized. |
| ERRCODE_OUT_OF_MEMORY | No memory available. |
| void osa_thread_attr_destroy | ( | OsaThreadAttr * | attr | ) |
Free memory for a thread attribute structure.
| attr | Attribute structure. The memory initialized in osa_thread_attr_init will be freed. |
| int osa_thread_attr_set_stack_size | ( | OsaThreadAttr * | attr, |
| size_t | size | ||
| ) |
Set the stack size for a thread attribute object.
| attr | A valid thread attribute object |
| size | The maximum stack size |
| ERRCODE_NO_ERROR | Function succeeded |
| ERRCODE_INVALID_ARGUMENT | Invalid attribute object or stack size outside of limits |
| int osa_thread_attr_get_stack_size | ( | const OsaThreadAttr * | attr, |
| size_t * | size | ||
| ) |
Retrieve the stack size for a thread attribute object.
| attr | A valid thread attribute object |
| size | An output parameter that will store the stack size |
| ERRCODE_NO_ERROR | Function succeeded |
| ERRCODE_INVALID_ARGUMENT | Invalid attribute object or NULL size pointer |
| int osa_thread_attr_set_sched_policy | ( | OsaThreadAttr * | attr, |
| OsaSchedPolicy | policy | ||
| ) |
Set the scheduling policy for a thread attribute object.
| attr | A valid thread attribute object |
| policy | The scheduling policy |
| ERRCODE_NO_ERROR | Function succeeded |
| ERRCODE_INVALID_ARGUMENT | Invalid attribute object or policy |
| int osa_thread_attr_get_sched_policy | ( | const OsaThreadAttr * | attr, |
| OsaSchedPolicy * | policy | ||
| ) |
Retrieve the scheduling policy for a thread attribute object.
| attr | A valid thread attribute object |
| policy | An output parameter that will store the policy |
| ERRCODE_NO_ERROR | Function succeeded |
| ERRCODE_INVALID_ARGUMENT | Invalid attribute object or NULL policy pointer |
| int osa_thread_attr_set_sched_priority | ( | OsaThreadAttr * | attr, |
| OsaSchedPriority | priority | ||
| ) |
Set the scheduling policy for a thread attribute object.
| attr | A valid thread attribute object |
| priority | The scheduling policy |
| ERRCODE_NO_ERROR | Function succeeded |
| ERRCODE_INVALID_ARGUMENT | Invalid attribute object or priority |
| int osa_thread_attr_get_sched_priority | ( | const OsaThreadAttr * | attr, |
| OsaSchedPriority * | priority | ||
| ) |
Retrieve the scheduling priority for a thread attribute object.
| attr | A valid thread attribute object |
| priority | An output parameter that will store the priority |
| ERRCODE_NO_ERROR | Function succeeded |
| ERRCODE_INVALID_ARGUMENT | Invalid attribute object or NULL priority pointer |
| int osa_thread_attr_set_sched_interval | ( | OsaThreadAttr * | attr, |
| uint32_t | interval | ||
| ) |
Set the scheduling interval for a thread attribute object.
| attr | A valid thread attribute object |
| interval | The scheduling interval, in milliseconds |
| ERRCODE_NO_ERROR | Function succeeded |
| ERRCODE_INVALID_ARGUMENT | Invalid attribute object or interval |
| int osa_thread_attr_get_sched_interval | ( | const OsaThreadAttr * | attr, |
| uint32_t * | interval | ||
| ) |
Retrieve the scheduling interval for a thread attribute object.
| attr | A valid thread attribute object |
| interval | An output parameter that will store the interval |
| ERRCODE_NO_ERROR | Function succeeded |
| ERRCODE_INVALID_ARGUMENT | Invalid attribute object or NULL interval pointer |
| int osa_thread_attr_set_name | ( | OsaThreadAttr * | attr, |
| const char * | name | ||
| ) |
Set the name to represent a thread in the attribute structure
| attr | A valid thread attribute object |
| name | Name for the thread (max of OSA_MAX_THREAD_NAME_LENGTH) |
| ERRCODE_NO_ERROR | Function succeeded |
| ERRCODE_INVALID_ARGUMENT | Invalid attribute object or NULL interval pointer |
| int osa_thread_create | ( | OsaThread * | thread, |
| const OsaThreadAttr * | attr, | ||
| void(*)(void *) | function, | ||
| void * | arg | ||
| ) |
Create a new thread of execution starting at the given function as an entry point. The new thread properties will be defined in 'attr'. Passing in NULL will use default properties. 'arg' is passed as the function argument to the new thread. The new thread may or may not be scheduled immediately.
| thread | Output argument that is returned to the caller that represents the ID of the newly-created thread. |
| function | The entry function for the new thread |
| attr | A valid thread attribute object or NULL |
| arg | The argument to be passed to the new thread entry point |
| ERRCODE_NO_ERROR | Function succeeded |
| ERRCODE_OUT_OF_MEMORY | Out of memory |
| ERRCODE_INVALID_ARGUMENT | Invalid input parameters. Thread attributes could be invalid. |
| ERRCODE_TRY_AGAIN | Exceeded system limits for threads. |
| ERRCODE_GENERAL_ERROR | Unexpected system error. |
| int osa_thread_destroy | ( | OsaThread | thread | ) |
| thread | The thread represented with this object will be destroyed. |
| ERRCODE_NO_ERROR | Function succeeded |
| ERRCODE_OUT_OF_MEMORY | Out of memory |
| ERRCODE_INVALID_ARGUMENT | Invalid input parameters. Thread attributes could be invalid. |
| ERRCODE_TRY_AGAIN | Exceed system limits for threads |
| ERRCODE_GENERAL_ERROR | Unexpected system error |
| OsaThread osa_thread_self | ( | void | ) |
| int osa_thread_join | ( | OsaThread | thread, |
| void ** | value | ||
| ) |
Wait for a given thread to terminate before continuing execution.
| thread | The thread to wait on for termination. |
| value | Not currently used, will be set to zero. |
| ERRCODE_NO_ERROR | Function succeeded |
| ERRCODE_INVALID_ARGUMENT | Invalid input parameters |
| ERRCODE_DEADLOCK | Two threads attempted to join with each other |
| ERRCODE_GENERAL_ERROR | Unexpected system error |
| void osa_thread_yield | ( | void | ) |
Force the currently running thread to yield the processor. This will cause another ready thread to be scheduled.
| void osa_thread_exit | ( | void * | value | ) |
Force the currently running thread to exit. This differs from osa_exit in that the OS/process does not exit on MQX/Linux, only the calling thread.
| value | Data to pass back upon exit |
| int osa_thread_get_id | ( | OsaThread | thread, |
| uint32_t * | tid | ||
| ) |
Return a unique identifier for a specific thread.
| thread | A valid thread object |
| tid | Output parameter holding the thread id |
| ERRCODE_NO_ERROR | Function succeeded |
| ERRCODE_INVALID_ARGUMENT | Invalid thread parameter |
| int osa_sched_set_policy | ( | OsaThread | thread, |
| OsaSchedPolicy | policy | ||
| ) |
Set the scheduling policy for a thread.
| thread | A valid thread object |
| policy | The scheduling policy |
| ERRCODE_NO_ERROR | Function succeeded |
| ERRCODE_INVALID_ARGUMENT | Invalid thread object or policy |
| int osa_sched_get_policy | ( | OsaThread | thread, |
| OsaSchedPolicy * | policy | ||
| ) |
Get the scheduling policy for a thread.
| thread | A valid thread object |
| policy | Output parameter to store the scheduling policy |
| ERRCODE_NO_ERROR | Function succeeded |
| ERRCODE_INVALID_ARGUMENT | Invalid thread object or policy |
| int osa_sched_set_priority | ( | OsaThread | thread, |
| OsaSchedPriority | priority | ||
| ) |
Set the scheduling priority for a thread.
| thread | A valid thread object |
| priority | The scheduling priority |
| ERRCODE_NO_ERROR | Function succeeded |
| ERRCODE_INVALID_ARGUMENT | Invalid thread object or priority |
| int osa_sched_get_priority | ( | OsaThread | thread, |
| OsaSchedPriority * | priority | ||
| ) |
Get the scheduling priority for a thread.
| thread | A valid thread object |
| priority | Output parameter to store the scheduling priority |
| ERRCODE_NO_ERROR | Function succeeded |
| ERRCODE_INVALID_ARGUMENT | Invalid thread object or priority |
| int osa_sched_set_rr_interval | ( | OsaThread | thread, |
| uint32_t | interval | ||
| ) |
Set the scheduling interval for a thread. This is only valid if the scheduling policy of the thread is set to round robin and the OS is MQX. It's not policy to adjust RR interval on Linux.
| thread | A valid thread object |
| interval | The scheduling interval in milliseconds. The task will execute for this much time before yielding the processor. |
| ERRCODE_NO_ERROR | Function succeeded |
| ERRCODE_INVALID_ARGUMENT | Invalid thread object or interval out of range |
| ERRCODE_NOT_SUPPORTED | Not supported (Linux only) |
| int osa_sched_get_rr_interval | ( | OsaThread | thread, |
| uint32_t * | interval | ||
| ) |
Get the scheduling interval for a thread.
| thread | A valid thread object |
| interval | Output parameter used to store the scheduling interval |
| ERRCODE_NO_ERROR | Function succeeded |
| ERRCODE_INVALID_ARGUMENT | Invalid thread object or interval out of range |
| ERRCODE_NOT_SUPPORTED | Not supported (Linux only) |
| int osa_thread_get_name | ( | OsaThread | thread, |
| char ** | name | ||
| ) |
Get the thread name string for a thread.
| thread | A valid thread object |
| name | name string |
| ERRCODE_NO_ERROR | Function succeeded |
| ERRCODE_INVALID_ARGUMENT | Invalid thread object or invalid name |
| ERRCODE_NOT_FOUND | No name string (MQX only) |
| int osa_thread_set_name | ( | OsaThread | thread, |
| const char * | name | ||
| ) |
Set the thread name string for a thread.
| thread | A valid thread object |
| name | name string |
| ERRCODE_NO_ERROR | Function succeeded |
| ERRCODE_INVALID_ARGUMENT | Invalid thread object or invalid name |
| ERRCODE_NOT_FOUND | No name string (MQX only) |