![]() |
Maestro Audio Framework
v 1.0
NXP Semiconductors
|
This file includes definitions for messages used by the Streamer library. More...
Macros | |
| #define | BLD_MESSAGE(msg, type) ((uint32_t)(((uint32_t)(msg)<<24)|((uint32_t)(type)))) |
| #define | MESSAGE_ID(msg) (uint32_t)((msg) >> 24) |
| #define | MESSAGE_TYPE(msg) (uint32_t)((msg) & 0xFFF) |
| #define | MSG_NULL (uint32_t)0 |
| #define | MSG_EOS BLD_MESSAGE(MESSAGE_EOS, 0) |
| MSG_EOS End of stream message from the pipeline. | |
| #define | MSG_ERROR_AUDIO BLD_MESSAGE(MESSAGE_ERROR, ERROR_VIDEO_FATAL) |
| MSG_ERROR_AUDIO Actual error type will be decoder dependent passed on in message data field. | |
| #define | MSG_ERROR_VIDEO BLD_MESSAGE(MESSAGE_ERROR, ERROR_AUDIO_FATAL) |
| MSG_ERROR_VIDEO Actual error type will be decoder dependent passed on in message data field. | |
| #define | MSG_WARNING_AUDIO BLD_MESSAGE(MESSAGE_ERROR, WARNING_AUDIO) |
| MSG_WARNING_AUDIO Actual warning type will be decoder dependent passed on in message data field. | |
| #define | MSG_WARNING_VIDEO BLD_MESSAGE(MESSAGE_ERROR, WARNING_VIDEO) |
| MSG_WARNING_VIDEO Actual warning type will be decoder dependent passed on in message data field. | |
| #define | MSG_INFO_VIDEO_BITRATE BLD_MESSAGE(MESSAGE_INFO, INFO_VIDEO_BITRATE) |
| MSG_INFO_VIDEO_BITRATE Message data will contain the bitrate in bits per second. | |
| #define | MSG_INFO_VIDEO_FRAMERATE BLD_MESSAGE(MESSAGE_INFO, INFO_VIDEO_FRAMERATE) |
| MSG_INFO_VIDEO_FRAMERATE Message data will contain the bitrate in frames per second. | |
| #define | MSG_INFO_VIDEO_TYPE BLD_MESSAGE(MESSAGE_INFO, INFO_VIDEO_TYPE) |
| MSG_INFO_VIDEO_TYPE Message data will contain the type of video. More... | |
| #define | MSG_INFO_AUDIO_BITRATE BLD_MESSAGE(MESSAGE_INFO, INFO_AUDIO_BITRATE) |
| MSG_INFO_AUDIO_BITRATE Message data will contain the bitrate in bits per second. | |
| #define | MSG_INFO_AUDIO_CHANNELS BLD_MESSAGE(MESSAGE_INFO, INFO_AUDIO_CHANNELS) |
| MSG_INFO_AUDIO_CHANNELS Message data will contain the number of channels supported. | |
| #define | MSG_INFO_AUDIO_SAMPLERATE BLD_MESSAGE(MESSAGE_INFO, INFO_AUDIO_SAMPLERATE) |
| MSG_INFO_AUDIO_SAMPLERATE Message data will contain the audio sampling rate in Hz. | |
| #define | MSG_INFO_AUDIO_TYPE BLD_MESSAGE(MESSAGE_INFO, INFO_AUDIO_TYPE) |
| MSG_INFO_AUDIO_TYPE Message data will contain the type of audio. More... | |
| #define | MSG_INFO_CODEC_INFO BLD_MESSAGE(MESSAGE_INFO, INFO_CODEC_INFO) |
| MSG_INFO_CODEC_INFO Message data will contain the pointer to a string of codec info. | |
| #define | MSG_INFO_DURATION BLD_MESSAGE(MESSAGE_INFO, INFO_DURATION) |
| MSG_INFO_DURATION Message data will contain the total duration of playback in milliseconds. | |
| #define | MSG_INFO_ALBUM BLD_MESSAGE(MESSAGE_INFO, INFO_ALBUM) |
| MSG_INFO_ALBUM Nothing in message data. More... | |
| #define | MSG_INFO_ARTIST BLD_MESSAGE(MESSAGE_INFO, INFO_ARTIST) |
| MSG_INFO_ARTIST Nothing in message data. More... | |
| #define | MSG_INFO_TITLE BLD_MESSAGE(MESSAGE_INFO, INFO_TITLE) |
| MSG_INFO_TITLE Nothing in message data. More... | |
| #define | MSG_INFO_GENRE BLD_MESSAGE(MESSAGE_INFO, INFO_GENRE) |
| MSG_INFO_GENRE Nothing in message data. More... | |
| #define | MSG_INFO_YEAR BLD_MESSAGE(MESSAGE_INFO, INFO_YEAR) |
| MSG_INFO_YEAR Nothing in message data. More... | |
| #define | MSG_INFO_TRACK BLD_MESSAGE(MESSAGE_INFO, INFO_TRACK) |
| MSG_INFO_TRACK Nothing in message data. More... | |
| #define | MSG_INFO_ALBUMART BLD_MESSAGE(MESSAGE_INFO, INFO_ALBUMART_IMAGE) |
| MSG_INFO_ALBUMART Message data will contain the total duration of playback in milliseconds. | |
| #define | MSG_INFO_POSITION BLD_MESSAGE(MESSAGE_INFO, INFO_POSITION) |
| MSG_INFO_POSITION Message data will contain the current time of playback in milliseconds. | |
| #define | MSG_STREAM_INFO_UPDATED BLD_MESSAGE(MESSAGE_INFO, INFO_STREAM_INFO_UPDATE) |
| MSG_STREAM_INFO_UPDATED Nothing in message data. More... | |
| #define | MSG_META_INFO_UPDATED BLD_MESSAGE(MESSAGE_INFO, INFO_META_INFO_UPDATE) |
| MSG_META_INFO_UPDATED Nothing in message data. More... | |
| #define | MSG_STREAM_ERROR BLD_MESSAGE(MESSAGE_INFO, INFO_ERROR) |
| MSG_STREAM_ERROR Message data will contain the error type. | |
| #define MSG_INFO_VIDEO_TYPE BLD_MESSAGE(MESSAGE_INFO, INFO_VIDEO_TYPE) |
Video type depends on the decoders supported.
| #define MSG_INFO_AUDIO_TYPE BLD_MESSAGE(MESSAGE_INFO, INFO_AUDIO_TYPE) |
Audio type depends on the decoders supported.
| #define MSG_INFO_ALBUM BLD_MESSAGE(MESSAGE_INFO, INFO_ALBUM) |
get tag function should be called to get the required tag.
| #define MSG_INFO_ARTIST BLD_MESSAGE(MESSAGE_INFO, INFO_ARTIST) |
get tag function should be called to get the required tag.
| #define MSG_INFO_TITLE BLD_MESSAGE(MESSAGE_INFO, INFO_TITLE) |
get tag function should be called to get the required tag.
| #define MSG_INFO_GENRE BLD_MESSAGE(MESSAGE_INFO, INFO_GENRE) |
get tag function should be called to get the required tag.
| #define MSG_INFO_YEAR BLD_MESSAGE(MESSAGE_INFO, INFO_YEAR) |
get tag function should be called to get the required tag.
| #define MSG_INFO_TRACK BLD_MESSAGE(MESSAGE_INFO, INFO_TRACK) |
get tag function should be called to get the required tag.
| #define MSG_STREAM_INFO_UPDATED BLD_MESSAGE(MESSAGE_INFO, INFO_STREAM_INFO_UPDATE) |
indicate that all stream information is updated
| #define MSG_META_INFO_UPDATED BLD_MESSAGE(MESSAGE_INFO, INFO_META_INFO_UPDATE) |
indicate that all metadata information is updated