![]() |
Maestro Audio Framework
v 1.0
NXP Semiconductors
|
Thread Attributes. More...
#include <osa_thread.h>
Data Fields | |
| size_t | stack_size |
| Stack size. | |
| OsaSchedPriority | priority |
| Scheduling priority. | |
| OsaSchedPolicy | policy |
| Scheduling policy. | |
| uint32_t | rr_interval |
| Scheduling interval. | |
| uint32_t | core |
| Target core. | |
| char | name [OSA_MAX_THREAD_NAME_LENGTH] |
| Thread name. | |
Stores attributes for a thread. The following should be included: