![]() |
Maestro Audio Framework
v 1.0
NXP Semiconductors
|
Streamer Message Type. More...
#include <streamer_api.h>
Data Fields | |
| uint32_t | id |
| Message Identifier, relative with STREAMER_MSG_ID. | |
| int | errorcode |
| Error Code. | |
| int8_t | pipeline_index |
| Pipeline Index. | |
| StreamPipelineType | pipeline_type |
| Pipeline Type. | |
| ELEMENT_PROPERTY_T | element_property |
| Property Structure. | |
| PipelineState | state |
| Pipeline State. | |
| StreamInfoType | query_type |
| Query Type. | |
| StreamData | query_data |
| Query Return Data. | |
| uint32_t | event_id |
| Event Identifier. | |
| int | event_data |
| Event Data. | |
| uint32_t | time_ms |
| Time. | |
| char * | in_dev_name |
| Input Device Name. | |
| char * | out_dev_name |
| Output Device Name. | |
| OsaMutex * | mutex |
| OsaCondition * | cond |
| Mutex to protect signal. | |
| bool * | processed |
| Signal to unlock wait for streamer response. | |
| int32_t * | ret |
| Flag to indicate streamer msg processed. | |
| void * | get_value |
| streamer message processing result | |
Structure for messages transmitted and received by the streamer task.