![]() |
Maestro Audio Framework
v 1.0
NXP Semiconductors
|
#include <streamer_api.h>
Data Fields | |
| uint32_t | value32u |
| uint16_t | value16u |
| uint8_t | value8u |
| int32_t | value32s |
| int16_t | value16s |
| int8_t | value8s |
| uint8_t | valuebool |
| StreamStringType | string |
| StreamImageType | image |
Holds the data related to a query or event