![]() |
eRPC API Reference
Rev. 1.8.1
NXP Semiconductors
|
This is the complete list of members for erpc::RPMsgBaseTransport, including all inherited members.
| get_rpmsg_lite_instance(void) | erpc::RPMsgBaseTransport | inline |
| hasMessage(void) | erpc::Transport | inlinevirtual |
| receive(MessageBuffer *message)=0 | erpc::Transport | pure virtual |
| RPMsgBaseTransport(void) (defined in erpc::RPMsgBaseTransport) | erpc::RPMsgBaseTransport | inline |
| s_initialized | erpc::RPMsgBaseTransport | protectedstatic |
| s_rpmsg | erpc::RPMsgBaseTransport | protectedstatic |
| send(MessageBuffer *message)=0 | erpc::Transport | pure virtual |
| setCrc16(Crc16 *crcImpl) | erpc::Transport | inlinevirtual |
| Transport(void) | erpc::Transport | inline |
| ~RPMsgBaseTransport(void) (defined in erpc::RPMsgBaseTransport) | erpc::RPMsgBaseTransport | inlinevirtual |
| ~Transport(void) | erpc::Transport | inlinevirtual |