![]() |
eRPC API Reference
Rev. 1.8.1
NXP Semiconductors
|
This is the complete list of members for erpc::Service, including all inherited members.
| getNext(void) | erpc::Service | inline |
| getServiceId(void) const | erpc::Service | inline |
| handleInvocation(uint32_t methodId, uint32_t sequence, Codec *codec, MessageBufferFactory *messageFactory)=0 | erpc::Service | pure virtual |
| m_next | erpc::Service | protected |
| m_serviceId | erpc::Service | protected |
| Service(uint32_t serviceId) | erpc::Service | inline |
| setNext(Service *next) | erpc::Service | inline |
| ~Service(void) | erpc::Service | inlinevirtual |