![]() |
eRPC API Reference
Rev. 1.8.1
NXP Semiconductors
|
Very basic transport to send/receive messages via SPI. More...
#include <erpc_spi_master_transport.h>
Inheritance diagram for erpc::SpiMasterTransport:
Collaboration diagram for erpc::SpiMasterTransport:Public Member Functions | |
| SpiMasterTransport (SPI_Type *spiBaseAddr, uint32_t baudRate, uint32_t srcClock_Hz) | |
| Constructor. More... | |
| virtual | ~SpiMasterTransport (void) |
| Destructor. | |
| virtual erpc_status_t | init (void) |
| Initialize SPI peripheral configuration structure with values specified in SpiTransport constructor. More... | |
Public Member Functions inherited from erpc::FramedTransport | |
| FramedTransport (void) | |
| Constructor. | |
| virtual | ~FramedTransport (void) |
| Codec destructor. | |
| virtual erpc_status_t | receive (MessageBuffer *message) override |
| Receives an entire message. More... | |
| virtual erpc_status_t | send (MessageBuffer *message) override |
| Function to send prepared message. More... | |
| virtual void | setCrc16 (Crc16 *crcImpl) override |
| This functions sets the CRC-16 implementation. More... | |
Public Member Functions inherited from erpc::Transport | |
| Transport (void) | |
| Constructor. | |
| virtual | ~Transport (void) |
| Transport destructor. | |
| virtual bool | hasMessage (void) |
| Poll for an incoming message. More... | |
Protected Attributes | |
| SPI_Type * | m_spiBaseAddr |
| uint32_t | m_baudRate |
| uint32_t | m_srcClock_Hz |
Protected Attributes inherited from erpc::FramedTransport | |
| Crc16 * | m_crcImpl |
| Mutex | m_sendLock |
| Mutex protecting send. | |
| Mutex | m_receiveLock |
| Mutex protecting receive. | |
Additional Inherited Members |
Very basic transport to send/receive messages via SPI.
| SpiMasterTransport::SpiMasterTransport | ( | SPI_Type * | spiBaseAddr, |
| uint32_t | baudRate, | ||
| uint32_t | srcClock_Hz | ||
| ) |
Constructor.
| [in] | spiBaseAddr | DSPI peripheral base address. |
| [in] | baudRate | Baudrate. |
| [in] | srcClock_Hz | Source clock. |
|
virtual |
Initialize SPI peripheral configuration structure with values specified in SpiTransport constructor.
| kErpcStatus_Success | Always returns success status. |
|
protected |
Base address of SPI peripheral used in this transport layer
|
protected |
Baud rate of SPI peripheral used in this transport layer
|
protected |
Source clock of SPI peripheral used in this transport layer