![]() |
eRPC API Reference
Rev. 1.8.1
NXP Semiconductors
|
This is the complete list of members for erpc::SpidevMasterTransport, including all inherited members.
| FramedTransport(void) | erpc::FramedTransport | |
| hasMessage(void) | erpc::Transport | inlinevirtual |
| init(void) | erpc::SpidevMasterTransport | |
| m_crcImpl | erpc::FramedTransport | protected |
| m_receiveLock | erpc::FramedTransport | protected |
| m_sendLock | erpc::FramedTransport | protected |
| m_speed_Hz | erpc::SpidevMasterTransport | protected |
| m_spidev | erpc::SpidevMasterTransport | protected |
| m_spidevHandle | erpc::SpidevMasterTransport | protected |
| receive(MessageBuffer *message) override | erpc::FramedTransport | virtual |
| send(MessageBuffer *message) override | erpc::FramedTransport | virtual |
| setCrc16(Crc16 *crcImpl) override | erpc::FramedTransport | virtual |
| SpidevMasterTransport(const char *spidev, uint32_t speed_Hz) | erpc::SpidevMasterTransport | |
| Transport(void) | erpc::Transport | inline |
| ~FramedTransport(void) | erpc::FramedTransport | virtual |
| ~SpidevMasterTransport(void) | erpc::SpidevMasterTransport | virtual |
| ~Transport(void) | erpc::Transport | inlinevirtual |