![]() |
eRPC API Reference
Rev. 1.8.1
NXP Semiconductors
|
Client side of TCP/IP transport. More...
#include <erpc_tcp_transport.h>
Inheritance diagram for erpc::TCPTransport:
Collaboration diagram for erpc::TCPTransport:Public Member Functions | |
| TCPTransport (bool isServer) | |
| Constructor. More... | |
| TCPTransport (const char *host, uint16_t port, bool isServer) | |
| Constructor. More... | |
| virtual | ~TCPTransport (void) |
| TCPTransport destructor. | |
| void | configure (const char *host, uint16_t port) |
| This function set host and port of this transport layer. More... | |
| virtual erpc_status_t | open (void) |
| This function will create host on server side, or connect client to the server. More... | |
| virtual erpc_status_t | close (bool stopServer=true) |
| This function disconnects client or stop server host. More... | |
Public Member Functions inherited from erpc::FramedTransport | |
| FramedTransport (void) | |
| Constructor. | |
| virtual | ~FramedTransport (void) |
| Codec destructor. | |
| virtual erpc_status_t | receive (MessageBuffer *message) override |
| Receives an entire message. More... | |
| virtual erpc_status_t | send (MessageBuffer *message) override |
| Function to send prepared message. More... | |
| virtual void | setCrc16 (Crc16 *crcImpl) override |
| This functions sets the CRC-16 implementation. More... | |
Public Member Functions inherited from erpc::Transport | |
| Transport (void) | |
| Constructor. | |
| virtual | ~Transport (void) |
| Transport destructor. | |
| virtual bool | hasMessage (void) |
| Poll for an incoming message. More... | |
Protected Member Functions | |
| virtual erpc_status_t | connectClient (void) |
| This function connect client to the server. More... | |
| virtual erpc_status_t | underlyingReceive (uint8_t *data, uint32_t size) |
| This function read data. More... | |
| virtual erpc_status_t | underlyingSend (const uint8_t *data, uint32_t size) |
| This function writes data. More... | |
| void | serverThread (void) |
| Server thread function. | |
Static Protected Member Functions | |
| static void | serverThreadStub (void *arg) |
| Thread entry point. More... | |
Protected Attributes | |
| bool | m_isServer |
| const char * | m_host |
| uint16_t | m_port |
| int | m_socket |
| Thread | m_serverThread |
| bool | m_runServer |
Protected Attributes inherited from erpc::FramedTransport | |
| Crc16 * | m_crcImpl |
| Mutex | m_sendLock |
| Mutex protecting send. | |
| Mutex | m_receiveLock |
| Mutex protecting receive. | |
Client side of TCP/IP transport.
| TCPTransport::TCPTransport | ( | bool | isServer | ) |
Constructor.
This function initializes object attributes.
| [in] | isServer | True when this transport is used for server side application. |
| TCPTransport::TCPTransport | ( | const char * | host, |
| uint16_t | port, | ||
| bool | isServer | ||
| ) |
Constructor.
This function initializes object attributes.
| [in] | host | Specify the host name or IP address of the computer. |
| [in] | port | Specify the listening port number. |
| [in] | isServer | True when this transport is used for server side application. |
| void TCPTransport::configure | ( | const char * | host, |
| uint16_t | port | ||
| ) |
This function set host and port of this transport layer.
| [in] | host | Specify the host name or IP address of the computer. |
| [in] | port | Specify the listening port number. |
|
virtual |
This function will create host on server side, or connect client to the server.
| kErpcStatus_Success | When creating host was successful or client connected successfully. |
| kErpcStatus_UnknownName | Host name resolution failed. |
| kErpcStatus_ConnectionFailure | Connecting to the specified host failed. |
|
virtual |
This function disconnects client or stop server host.
| [in] | stopServer | Specify is server shall be closed as well (stop listen()) |
| kErpcStatus_Success | Always return this. |
|
protectedvirtual |
This function connect client to the server.
| kErpcStatus_Success | When client connected successfully. |
| kErpcStatus_Fail | When client doesn't connected successfully. |
|
protectedvirtual |
This function read data.
| [in,out] | data | Preallocated buffer for receiving data. |
| [in] | size | Size of data to read. |
| kErpcStatus_Success | When data was read successfully. |
| kErpcStatus_ReceiveFailed | When reading data ends with error. |
| kErpcStatus_ConnectionClosed | Peer closed the connection. |
Implements erpc::FramedTransport.
|
protectedvirtual |
This function writes data.
| [in] | data | Buffer to send. |
| [in] | size | Size of data to send. |
| kErpcStatus_Success | When data was written successfully. |
| kErpcStatus_SendFailed | When writing data ends with error. |
| kErpcStatus_ConnectionClosed | Peer closed the connection. |
Implements erpc::FramedTransport.
|
staticprotected |
Thread entry point.
Control is passed to the serverThread() method of the TCPTransport instance pointed to by the arg parameter.
| arg | Thread argument. The pointer to the TCPTransport instance is passed through this argument. |
|
protected |
If true then server is using transport, else client.
|
protected |
Specify the host name or IP address of the computer.
|
protected |
Specify the listening port number.
|
protected |
Socket number.
|
protected |
Pointer to server thread.
|
protected |
Thread is executed while this is true.