![]() |
eRPC API Reference
Rev. 1.8.1
NXP Semiconductors
|
This is the complete list of members for erpc::Thread, including all inherited members.
| getCurrentThread(void) | erpc::Thread | static |
| getCurrentThreadId(void) | erpc::Thread | inlinestatic |
| getName(void) const | erpc::Thread | inline |
| getThreadId(void) const | erpc::Thread | inline |
| init(thread_entry_t entry, uint32_t priority=0, uint32_t stackSize=0) | erpc::Thread | |
| operator==(Thread &o) | erpc::Thread | |
| setName(const char *name) | erpc::Thread | inline |
| sleep(uint32_t usecs) | erpc::Thread | static |
| start(void *arg=0) | erpc::Thread | |
| Thread(const char *name=0) | erpc::Thread | |
| Thread(thread_entry_t entry, uint32_t priority=0, uint32_t stackSize=0, const char *name=0) | erpc::Thread | |
| thread_id_t typedef | erpc::Thread | |
| threadEntryPoint(void) | erpc::Thread | protectedvirtual |
| ~Thread(void) | erpc::Thread | virtual |