![]() |
eRPC API Reference
Rev. 1.8.1
NXP Semiconductors
|
This is the complete list of members for erpc::UsbCdcTransport, including all inherited members.
| FramedTransport(void) | erpc::FramedTransport | |
| hasMessage(void) | erpc::Transport | inlinevirtual |
| init(void) | erpc::UsbCdcTransport | virtual |
| m_crcImpl | erpc::FramedTransport | protected |
| m_receiveLock | erpc::FramedTransport | protected |
| m_rxSemaphore | erpc::UsbCdcTransport | protected |
| m_sendLock | erpc::FramedTransport | protected |
| m_txSemaphore | erpc::UsbCdcTransport | protected |
| receive(MessageBuffer *message) override | erpc::FramedTransport | virtual |
| rx_cb(void) | erpc::UsbCdcTransport | |
| send(MessageBuffer *message) override | erpc::FramedTransport | virtual |
| setCrc16(Crc16 *crcImpl) override | erpc::FramedTransport | virtual |
| Transport(void) | erpc::Transport | inline |
| tx_cb(void) | erpc::UsbCdcTransport | |
| UsbCdcTransport(serial_handle_t serialHandle, serial_manager_config_t *serialConfig, serial_port_usb_cdc_config_t *usbCdcConfig, uint8_t *usbRingBuffer, uint32_t usbRingBufferLength) | erpc::UsbCdcTransport | |
| ~FramedTransport(void) | erpc::FramedTransport | virtual |
| ~Transport(void) | erpc::Transport | inlinevirtual |
| ~UsbCdcTransport(void) | erpc::UsbCdcTransport | virtual |