![]() |
eRPC API Reference
Rev. 1.8.1
NXP Semiconductors
|
Include dependency graph for erpc_client_manager.h:
This graph shows which files directly or indirectly include this file:Go to the source code of this file.
Classes | |
| class | erpc::ClientManager |
| Base client implementation. More... | |
| class | erpc::RequestContext |
| Encapsulates all information about a request. More... | |
Typedefs | |
| typedef void(* | client_error_handler_t) (erpc_status_t err, uint32_t functionID) |